×
Siemens Industry Online Support
Siemens AG
Entry type: Application example, Entry ID: 109739689, Entry date: 06/29/2017
(2)
Rate

Communication with S7 CPU via KNX Gateway

  • Entry
  • Associated product(s)
This application example shows, how you configure communication via a gateway between SIMATIC S7 CPU and a KNX device via the KNX bus.

Task
Gateways enable communication between two networks/bus systems that use different communications protocols.
KNX is a fieldbus for building automation. Technically, KNX is the successor to the European Installation Bus (EIB), adding communication mechanisms and transmission media.

The task is to establish, using a KNX gateway, a communication connection between an S7 CPU via PROFINET (PN) and a KNX device via the KNX bus.

The figure below provides an overview of the automation task.


Figure 1

Solution
Representing all SIMATIC controllers, this solution uses an S7-1200 CPU. The diagrammatic representation below shows the most important components for communication between an S7-1200 CPU and a KNX network using the “Triple-X PROFINET + KNX” universal gateway from MBS GmbH.



Figure 2

Advantages

The solution presented here offers the following advantages:
  • Easy adaptation to other controller families. Representing all other SIMATIC controllers with a PROFINET IO interface, this solution uses the S7-1200 CPU.
  • Easy adaptation when expanding plants. The gateway is configured directly in the gateway’s integrated web server.
  • Integration of the gateway as a PROFINET IO device via a GSD file.
  • Gateway as distributed I/O with up to 340 bytes of input and 340 bytes of output.
  • Up to 2500 data points possible for communication between PROFINET and KNX.

Downloads
  Documentation (2,5 MB)
 Registrierung notwendig  109739689_KNX_S7_PROJ_V10.zip (589,0 KB) 
 Registrierung notwendig  109739689_KNX_Gateway_RestoreFile_V10.zip (4,2 KB) 
 Registrierung notwendig  109739689_KNX_ETS5_PROJ_V10.zip (1,2 MB) 

Further information
Homepage of the company MBS GmbH




Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.