×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109740115, Entry date: 11/20/2017
(4)
Rate

Determination of suitable hardware for the Process Historian 2014 with the "PH-HWAdvisor" tool

  • Entry
  • Associated product(s)
The Process Historian is used for long-term archiving of process data and messages. To ensure optimum operation and constant availability of data, the Process Historian 2014 has been subjected to a special delivery release since March 2016, which needs the determination of the suitable hardware.


Since 5th of September 2016 the obligatory consultation of the Systems Support has been replaced by the following process and the "PH-HWAdvisor" tool.

The "PH-HWAdvisor" tool guides you through a catalog of questions on the individual requirements of your PCS 7 project and provides a results protocol with the recommended hardware, which has to be sent to the responsible Product Manager for getting the order approval.

Follow these steps:

  1. Download the tool.
  2. Unzip and start the tool.
  3. Fill in the fields provided and start the evaluation.
  4. Send the signed protocol to the specified address in order to obtain order approval for the Process Historian 2014.

Responsible Product Manager for the order approval
Mr. Dr. Dino Drinjakovic
dino.drinjakovic@siemens.com 

Documentation and Tool
  Instructions (PH-HWAdvisor) (795,1 KB)
 Registrierung notwendig  Tool (PH-HWAdvisor) (123,5 KB)

Further information
Installation, Operation and Maintenance of Process Historian/Information Server in a PCS 7 Environment

Last Changes
New tool version V3.1:

  • SIMATIC DCS Infrastructure Service note in the report
  • SIMATIC BATCH note in the report
  • Default settings in HDD price dialog
  • Updated to PCS 7 V9.0
      
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.