×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109740141, Entry date: 06/06/2019
(11)
Rate

Multiuser Engineering in TIA Portal

  • Entry
  • Associated product(s)
With Multiuser Engineering in TIA Portal, you can work with multiple users together and simultaneously on a project. By processing different objects in parallel within a multiuser project, you can significantly shorten the project planning and commissioning times.

TIA Portal V14 and higher provides you with various server constellations for the functionality of multiuser engineering. This application example describes the parallel processing of projects with a "temporary multiuser server", in which the server functionality is realized on a dedicated server. The multiuser server projects are also stored on the dedicated server.

In order to be able to work simultaneously with several agents in a multiuser server project within the framework of multiuser engineering, each agent must create their own local session. In the local session, the respective editor can insert his changes and then check these changes into the multiuser server project and publish them. After check-in, the changes from the local session are available again to all editors in the server project.

In addition to multiuser engineering, multiuser commissioning allows you to carry out joint commissioning in a team just as conveniently.

The following figure shows the server constellation "Multiuser server as dedicated server".



This application example describes the following aspects:
  • Configuring and managing a multiuser server
  • Creating and managing multiuser server projects
  • Creating and managing local sessions
  • Marking and checking in objects in a local session
  • Updating a local session
  • Exporting a local session as single-user project
  • Editing objects in the server project view
  • Joint commissioning with multiuser commissioning
  • Joint commissioning without multiuser commissioning


Documentation
  Documentation (2,3 MB)


Last Changes
Update to TIA Portal Multiuser Engineering V15



Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.