×
Siemens Industry Online Support
Siemens AG
Entry type: Application example, Entry ID: 109740160, Entry date: 09/22/2016
(7)
Rate

Communication with S7-CPU via DALI Gateway

  • Entry
  • Associated product(s)
This application example shows how to configure a communication between a SIMATIC CPU and a DALI network with the help of a gateway.

Gateways enable the communication between two networks that use different communication protocols.DALI (Digital Addressable Lighting Interface) is a network protocol to control lighting devices in facility automation.
The task is to create a communication connection between a SIMATIC CPU and a DALI device via a PROFINET interface using a DALI gateway.


Picture 1
 

Solution
An S7-1200 CPU is used in place of all SIMATIC controllers. The figure below shows the most important components for the communication between an S7-1200 CPU and the “multi PROFINET + DALI” gateway by MBS GmbH.


Picture 2

Advantages

  • The application example can simply be adjusted to other controller families.
  • The application example can be simply adjusted for plant expansions.
  • Configuring and commissioning the gateways does not require any additional software. Standard tools such as a simple text editor are sufficient. The configuration can be edited directly in the gateway.

Documentation and project example
  Documentation (1,9 MB)
 Registrierung notwendig  Project for STEP 7 V13 SP1 (2,2 MB)
 Registrierung notwendig  Gateway Code (8,2 KB)

Further information
Homepage of the MBS GmbH

Last modification
New publication


Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.