×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109740160, Entry date: 09/22/2016
(7)
Rate

Communication with S7-CPU via DALI Gateway

  • Entry
  • Associated product(s)
This application example shows how to configure a communication between a SIMATIC CPU and a DALI network with the help of a gateway.

Note:
Please note that a DALI V2 Multimaster module is also available for ET 200SP.
For more information, see the product release 109769177
An application example for the use of this DALI V2 Multimaster module is also available 109771151

Gateways enable the communication between two networks that use different communication protocols.DALI (Digital Addressable Lighting Interface) is a network protocol to control lighting devices in facility automation.
The task is to create a communication connection between a SIMATIC CPU and a DALI device via a PROFINET interface using a DALI gateway.


Picture 1
 

Solution
An S7-1200 CPU is used in place of all SIMATIC controllers. The figure below shows the most important components for the communication between an S7-1200 CPU and the “multi PROFINET + DALI” gateway by MBS GmbH.


Picture 2

Advantages

  • The application example can simply be adjusted to other controller families.
  • The application example can be simply adjusted for plant expansions.
  • Configuring and commissioning the gateways does not require any additional software. Standard tools such as a simple text editor are sufficient. The configuration can be edited directly in the gateway.

Documentation and project example
  Documentation (2,3 MB)
 Registrierung notwendig  Project for STEP 7 V15.1 (385,2 KB)
 Registrierung notwendig  Gateway Code (8,2 KB)

Further information
Homepage of the MBS GmbH


Last modification

Update TIA Portal V15.1


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.