SINAMICS S120 Firmware Version 4.8 HF6
-
Entry
-
Associated product(s)
Description |
---|
The version name on the memory card (CF) is SINAMICS S120 V04.08.00.06 The internal version number of the firmware is SINAMICS S120 V04.80.65.35. When upgrading, please observe the instructions for the firmware update. |
Third-party software - Licensing terms and copyright Information |
---|
You can find the copyright information for third-party software contained in this product, particularly open source software, as well as applicable licensing terms of such third-party software in the READ_OSS.HTM file. The information and the license terms in the READ_OSS.HTM file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party. Certain license conditions of third-party software components used in this product may require Siemens to provide you with the source code and additional information for such components. In most cases, Siemens provides this information on or with the device. In case Siemens is technically unable to do so, you may request a copy of of this OSS source code against payment of shipping and handling charges. Please send your request to the address provided at the end of this section. Siemens AG |
Restrictions of the SINAMICS S120 |
---|
![]() |
Corrected functional Restrictions for SINAMICS S120 for CU320-2 and CU310-2 |
---|
Instructions to update the firmware of the SINAMICS S120 CU320-2 and CU310-2 |
---|
![]() |
SINAMICS S120 firmware version V4.8 HF6 for the CU320-2 und CU310-2 |
---|
The following software can be downloaded:
Note: Alternatively, a new memory card (CF) with the following order number can be used:
|
List of faults and alarms |
---|
The "alarmlist_*.xml" are not necessary for the correct operation of the firmware and the associated STARTER. They only contain a text-based export of the "Alarm messages" of the S120 in the "xml" format (this format guarantees a correct text-based representation, independent of the wide range of fonts that exist worldwide; this means that they can be converted error-free into other formats).
|
GSD files for project integration into the PROFIBUS configuring tool |
---|
The PROFINET GSDML files are stored under the following path on the SINAMICS S120 CompactFlash card: ..\SIEMENS\SINAMICS\DATA\CFG They can also be downloaded: (see 49216293) |
GSDML files for project integration into the PROFINET configuring tool |
---|
The PROFINET GSDML files are stored under the following path on the SINAMICS S120 CompactFlash card: ..\SIEMENS\SINAMICS\DATA\CFG They can also be downloaded: (see 49217480) |
EDS files for project integration into the CANopen configuring tool |
---|
see 48351511 |
STARTER |
---|
Within the framework of the Firmware Version V4.8, the new STARTER V4.5 version will also be provided (see 109740000). |
- German
Entry belongs to product tree folder(s):
- You have a technical question / problem: Ask the Technical Support
- You want to discuss in our forum and exchange experiences with other users
- You want to create CAx data for one or more products
- You would like to send us feedback on this Entry