×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109740240, Entry date: 06/12/2017
(10)
Rate

How do you assign PROFIsafe addresses so that they are unique network-wide and CPU-wide?

  • Entry
  • Associated product(s)
Various plant configurations have different requirements for the network-wide and CPU-wide uniqueness of PROFIsafe addresses. This document explains the requirements taking different configuration examples.

The assignment of unique PROFIsafe addresses in the viewed configuration depends on

  • The F IO used (PROFIsafe address type 1 or 2)
  • The interface used (integrated PN interface or communication module)
  • The network infrastructure (switches, PN/PN coupler, for example)

The document provided below shows the different plant configurations and explains the assignment of a network-wide and CPU-wide unique PROFIsafe address. The view starts with two plant parts with F IO of PROFIsafe address types 1 and 2, and a central F IO (see figure below):


Fig. 01

Documentation
  Documentation (1,2 MB) 

Last change
Addition of a configuration with routing option.



Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.