×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109740338, Entry date: 10/05/2016
(2)
Rate

How do you prepare STEP 7 for the export of topology data/flows for SINETPLAN?

  • Entry
  • Associated product(s)
Procedure for storing topology files/data flows in the STEP 7 project if SINETPLAN is not installed

Description
If SINETPLAN is not installed on a PC with STEP 7, then STEP 7 does not store any topology files/data flows in the STEP 7 project which are needed for subsequent import into SINETPLAN.

You have the options below to meet the requirements that STEP 7 stores the data required for SINETPLAN in the project.

  1. You manually change the necessary keys in the Registry as described in the documentation/Help for SINETPLAN (not recommended).

  2. On the PC with STEP 7 you execute one of the Reg files available in the "Download" section:

    - "Regentry_for_STEP7_Classic_32Bit.reg" for the 32-bit version of Windows

    - "Regentry_for_STEP7_Classic_64Bit.reg" for the 64-bit version of Windows

Download
The two Reg files are in the ZIP file below:
 Registration required Regentry_for_STEP7_Classic.zip (1 KB)

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.