×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109740340, Entry date: 09/30/2016
(31)
Rate

Delivery Release for SIMATIC STEP 7 Professional / Basic V14

  • Entry
  • Associated product(s)
The innovative control programming for scalable solutions in the TIA Portal.

SIMATIC STEP 7 Professional / Basic V14

The innovative control programming for scalable solutions in the TIA Portal.

SIMATIC STEP 7 V14 Professional / Basic offers impressive, innovative engineering functions for flexible and fast implementation of control tasks.

The expansion of S7-1500 controllers with the T-CPU family (Technology) and CPU 1518(F)-4 PN/DP ODK, for combining C/C++ code with the STEP 7 languages, for example, as well as significant performance improvements in the engineering software round off version 14.

You can find the latest news on additional TIA Portal products at the following site: 109739471

Highlights SIMATIC STEP 7 V14

STEP 7 V14 includes new functions for all phases of the engineering workflow. An overview of the new functions is available here:  Registrierung notwendig  STEP_7_V14_new_functions.pdf (4,1 MB) 


Hardware configuration

  • Support for the S7-1500 T-CPU series with the Motion Control functions "Absolute synchronous operation" and "Camming".
  • Support for new CPU 1518(F)-4 PN/DP ODK (Open Development Kit), which enables you to connect to the user program via C/C++ functions created in SIMATIC ODK 1500S109741201
  • Support for CPU 1516pro (F)-2 PN109739235

  • Support of the new S7-1500 Fail-safe Software Controller 109483757 

  • Support of the new Fail-safe CPU 1212 FC 109739232

  • Grouping IO devices / other devices in the project tree enables you to quickly find and technologically merge devices.

  • The arrangement of the devices in the topological view can now be synchronized with the network view.
  • Custom profiles in the hardware catalog can now be defined for quick and easy access to frequently used modules.


Editors for programming languages

  • Separate editors are available for the new technology objects, cams, cam tracks and measuring inputs. There is also a convenient cam editor for S7-1500T controllers.
  • SCL networks can now be inserted in a LAD/FBD block.
  • "Regions" can be used to improve the structure and navigation in SCL code.
  • Block parameters can be hidden when the block is called in LAD or FBD.
  • The comparison of PLC programs was fundamentally revised and enables fast and convenient source code comparison with numerous filter options.
  • Networks are automatically displayed in the editors for LAD/FBD/STL as they appeared the last time the block closed.

Language innovations

  • You can transfer ARRAYs of variable lengths as block parameters using ARRAY[*].

  • In the block interface, multiple instances can be declared in ARRAYs and invoked in loops. This results in a substantial reduction of the code, better readability and

    more efficient programming during the execution of identical program objects.

  • The DB_ANY data type can also be used for technology objects. This enables more flexible handling of technology objects in the program. An "Array of DB_ANY", for example, can show

    a list of positioning axes.

  • Instances can be passed as a parameter in the InOut interface,

    so that only a dedicated instance must be selected for the call.

  • Alarm texts and comments for up to 3 languages can be downloaded to the S7-1500 PLC and changed

    online.

Messages / Diagnostics

  • Using the new "Get_Alarm" instruction, alarms can be directly read from the alarm server of the S7-1500 CPU and, for example, sent to a higher-level alarm system (e.g. control system).
  • For the instruction "GET_DIAG", the diagnostics data in the DIS structure are output in mode 1.Bit 15 of the IOState parameter of this structure returns the signal state "1" when a network/hardware error occurs.

Trace

  • The trace function makes it possible to display different measurements in a common chart

    ("superimposed measurements").

  • Once the trace is completed, measurements can also be retentively stored on the memory card

    and automatically restarted if required.

Online functions

  • Restructuring of the toolbar in the DB editor and the possibility to re-initialize complete DBs with defined starting values.
  • Structured tags in the block can be monitored in their call environment directly in the Inspector window.

System functions

  • The new global search allows project-spanning searching for PLC and HMI objects.The search results can also be restricted by filters. A "GoTo" function is also available.
  • TIA Portal settings can be exported or imported and stored on a central server. For example, if a server path is available, the stored settings are automatically applied as "defaults" each time the TIA Portal starts. Innovated help/information system with tab technology, improved search function and the option to filter information by device series.

  • Innovated help/information system with tab technology, improved search function and the

    option to filter information by device series.

  • The new cross-reference list provides a quick overview of how objects and devices are used within the project.
    • Support for overlapping access (PLC tags)
    • Support of know-how protected blocks
    • Access to individual elements of an ARRAY
    • Representation of objects found in both HMI and PLC devices
    • Free input in search for objects in the cross-reference list
    • Various filter options
  • Updates can be made available in corporate networks conveniently and centrally.

    Proprietary servers can be configured with the TIA Automation Corporate Configuration Tool. The available updates/support packages are stored on the server and thus made available to users.

TIA Portal Openness

You can use the API interface of WinCC and STEP 7 in the TIA Portal to integrate the TIA Portal in your development environment and automate your engineering tasks. Write your own applications with external development environments, for example, a code generator for HMI screens and PLC blocks. These functions are activated by installing the "TIA Portal Openness" add-on package. It is available on the product DVD in the folder Support/Siemens_TIA_Openness_V14.exe

S7-PLCSIM

  • Fast start of S7-PLCSIM in compact mode and without a simulation project.
  • Devices can be exchanged in the simulation project, so that existing SIM tables and sequence entries can continue to be used easily.

  • Recordings of CPU traces can be imported as sequences.

  • Sequences can be started automatically based on a trigger condition.

  • Sequences can be temporarily disabled.

  • Distributed IO devices can be simulated in the device view.

Motion control applications

  • Pre-configured and integrated connection and configuration of the SINAMICS V90 PN drive to a Motion Control technology object of SIMATIC S7-1500.
  • Automatic data synchronization between controller and drive.

SIMATIC STEP 7 V14 Product information

Editions

  • SIMATIC STEP 7 Professional V14

is the high-performance, integrated engineering system for the latest SIMATIC controller S7-1500, S7-1200, S7-300, S7-400, WinAC and ET 200 CPU. S7-PLCSIM for simulation of the S7-1500, S7-1200 CPU as well as SIMATIC WinCC Basic for configuration of Basic Panels and SINAMICS Startdrive for configuration of drives are included in the product package.

  • SIMATIC STEP 7 Basic V14

is the easy-to-use engineering system for the small, modular SIMATIC S7-1200 controller and the associated I/Os. It includes S7-PLCSIM for simulating the S7-1200 CPU and SIMATIC WinCC Basic for configuration of the SIMATIC Basic Panels.

System requirements

STEP 7 Professional / Basic V14 are released for use with the following operating systems (64-bit only):
  • Microsoft Windows 7 Home Premium SP1 (STEP 7 Basic only)
  • Microsoft Windows 7 Professional SP1
  • Microsoft Windows 7 Enterprise SP1
  • Microsoft Windows 7 Ultimate SP1
  • Microsoft Windows 8.1 (STEP 7 Basic only)
  • Microsoft Windows 8.1 Professional
  • Microsoft Windows 8.1 Enterprise
  • Microsoft Server 2008 R2 StdE SP1 (STEP 7 Professional only)
  • Microsoft Server 2012 R2 StdE

Note: Operating system support of Windows 10 is scheduled for V14 Service Pack 1.

The following table shows the recommended hardware for operating STEP 7.

HardwareRecommendation
ComputerSIMATIC Field PG M5 Advanced or higher (or comparable PC)
ProcessorIntel® Core™ i5-6440EQ (up to 3.4 GHz)
RAM16 GB or more (for large projects 32 GB)
Hard diskSSD with at least 50 GB of free space
Network1 GB (for multi-user)
Screen15.6" full HD display (1920 x 1080 or larger)

 

Compatibility with other products

STEP 7 Professional / Basic V14 works together with WinCC, Startdrive and Scout TIA V14 in a single framework.

STEP 7 Professional / Basic V14 (including WinCC Basic V14) can be installed on a PC in parallel with other versions
of STEP 7 V11 up to V13 SP1, STEP 7 V5.5 SP4, STEP 7 Micro/WIN V4.0 SP9, WinCC flexible 2008 SP3 and WinCC (as of V7.3).

A project upgrade to TIA Portal V14 is performed exclusively on the basis of TIA Portal V13 SP1 projects (last update recommended). To offer you the best possible support in this respect, we supply the current version of V13 SP1 within the STEP 7 V14 products. Compatibility mode is not supported.

Supported virtualization platforms

  • VMware vSphere Hypervisor (ESXi) 5.5 as of Update 2
  • VMware Workstation 11
  • VMware Player Pro 7.0
  • Microsoft Windows Server 2012 R2 Hyper-V

Supported operating systems for virtualization platforms as the host operating system

  • Windows 7 Professional/Ultimate/Enterprise (64-bit)
  • Windows Server 2008 R2 (64-bit)
  • Windows Server 2012 R2 (64-bit)
  • Windows 8.1 Professional/Enterprise (64-bit)

The following virus scanners were tested with STEP 7 V14:

  • Symantec Endpoint Protection 12.1
  • Trend Micro Office Scan Corporate Edition 11.0
  • McAfee VirusScan Enterprise 8.8
  • Kaspersky Anti-Virus 2016
  • Windows Defender (as of Windows 8.1)
  • Qihoo "360 Safe Guard" 9.7

Ordering data

The products with article numbers (order numbers) are listed in the attached file.

 Registrierung notwendig  step_7_v14_orderlist.xls (41,0 KB)


The new TIA Portal / STEP 7 add-on packages included in the list are described in more detail in the following entry: 109739471 


Software Update Service (SUS) as download

All automation software updates on the day of publication, available complete for all applications and independent of location - worldwide! Make the switch to the Software Update Service (SUS) as download now

    Trial software download

    Here you can download a trial version for SIMATIC STEP 7 Basic and Professional V14 and test it for 21 days. 109740158

    Readme file

    You can find additional information on STEP 7 V14 Basic/Professional in the attached Readme file.
    You can view this file in the portable document format (.pdf):

    Informational material

    TitleLink
    Online Support - Technical information on the TIA Portal65601780
    Programming Guideline for S7-1200 / S7-150067582299
    Comparison list for programming languages86630375

    Requesting TIA Portal Openness enabler and usage file

    Note: Enabler and usage files are version independent. You can continue using any existing enabler and usage files with TIA Portal V14.

    109741472




      Security information
      In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
      https://www.siemens.com/cybersecurity#Ouraspiration.