×
Siemens Industry Online Support
Siemens AG
Type de contribution : Exemple d’application ID de la contribution : 109740344, Date de la contribution : 21/03/2017
(6)
Évaluer

Automated creation of the SIMIT simulation model with COMOS planning and engineering data

  • Contribution
  • Concerne le/les produits(s)
This application example is a "best practice" example and shows you how to import COMOS planning data into SIMIT and automatically create your simulation model.

Objective of this COMOS P&ID application example
Digitization is currently ubiquitous and inextricably linked to the generation and processing of information. The construction of a fully-integrated data landscape is one of the most important prerequisites for the digital process creation.

This application example is a "best practice" example and shows you how to import COMOS planning data into SIMIT and automatically create your simulation model.

Optimized engineering workflows in automation and the shortest possible set-up and commissioning times for new production lines enable fast and high-quality products on the market.

This application example gives you the first insight into how you can implement this requirement with SIMIT and COMOS. The main focus is on the COMOS plug-in "SIMIT interface" and the SIMIT function "Generic import" for automatic model creation.

 
 
Validity
COMOS V10.2.0 and V10.2.1 with SIMIT V9.0 SP1

Attention
As of COMOS V10.2.2 the description doesn't work any more, because there was a change in the interface. An Update is planned.

Documentation and preconfigured project data
  Automated creation of the SIMIT simulation model with COMOS planning data (3,4 MB)
 Registrierung notwendig  COMOS example project based on iDB (217,7 MB) 
 
 
Further Information

Further application examples to the topic
Application Example - Controlled plant engineering from the outset with COMOS FEED
Application Example - Fast and easy generation of Piping and Instrumentation Diagrams with COMOS P&ID using a practical example
Application Example - Integrated Engineering with COMOS and SIMATIC PCS 7 using a practical example
Application Example - Simulation with SIMIT and SIMATIC PCS 7 using a practical example 

Further videos to the topic
Video - Integrated Engineering on the basis of COMOS with SIMATIC PCS 7 and SIMIT Simulation (Video)
  

You can find more useful content like FAQs, application examples, manuals, forum entries, videos, services or contact persons on the following topic pages:
www.siemens.com/onlinesupport/pcs7 
www.siemens.com/onlinesupport/comos 

Product pages
www.siemens.com/simit 
www.siemens.com/pcs7
www.siemens.com/comos 
Notes relatives à la sécurité
La protection des installations, systèmes, machines et réseaux contre les cyber-menaces nécessite la réalisation (et le maintien continu) d'un concept global de sécurité IT à la pointe de la technique. Les produits et solutions Siemens ne constituent qu'un élément d'un tel concept. Pour plus d’informations sur la cyber-sécurité, rendez-vous sur
https://www.siemens.com/cybersecurity#Ouraspiration.
Aide pour la statistique
Cette fonction permet de délivrer les identifiants des résultats de la recherche selon la quantité souhaitée (format .txt).

Générer une liste
Copier l'URL
Afficher cette page dans le nouveau design
Poste de commande mySupport
Liens connexes