×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109740620, Entry date: 10/02/2018
(0)
Rate

Equipment Phases for standardized automation of batch processes in the Chemical Industry

  • Entry
  • Associated product(s)
The Batch EPH contain the SFC and CM instances for standardized start-up and operation of the plant section.

Introduction
The standardization of automation technology for process plants, e.g. in the chemical industry, is a major challenge. Different process steps and procedures, different equipment and flexibility in production make this task more challenging.
One solution is to structure the discontinuous plant according to the physical model of ISA-88 / IEC 61512. The lower four levels, i.e. plant, plant section, plant section and individual control unit, are specified here. A plant always consists of subsystems. The subsystems, in turn, can contain standardized equipment phases based on technical functions (Control Modules, abbreviated CM) and controlled via SFC. A technical function consists of both the user program and the physical setup.

This application example contains standardized automation functions in the form of Batch Equipment Phases, abbreviated Batch EPH, as Software. Typicals, which are provided as multi-project in SIMATIC PCS 7.

The following advantages result from their use:

  • Reduction of the skills required for application development
  • Reduction of the project planning workload
  • Standardized structures
  • High degree of standardization and thus reduced upgrade costs
  • Flexible structure and customization of partial automation solutions





Documentation and sample project for PCS 7 V9.0
  Documentation (3,7 MB)
  Show mobile friendly
 Registrierung notwendig  Sample project (122,1 MB)
   
Weitere Informationen
Equipment Modules for SIMATIC PCS 7 using the example of the Chemical Industry
PCS 7 Unit Template "Distillation Column" using the example of the Chemical Industry
PCS 7 Unit Template "Stirred Tank Reactor" using the example of the Chemical Industry
PCS 7 Unit Template "Fermenter" using the example of the Chemical Industry
PCS 7 Unit Template "Dryer" using the example of the Chemical Industry
PCS 7 Unit Template "Polymerization Reactor" using the example of the Chemical Industry
Templates for specification of technical functions with SFC Types in SIMATIC PCS 7 

Ergänzende Suchbegriffe
Equipment Module, Modules, Equipment Phases

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.