×
Siemens Industry Online Support
Siemens AG
Entry type: Download, Entry ID: 109740858, Entry date: 09/21/2016
(0)
Rate

Download of firmware SCALANCE M-800 / S615 V04.02

  • Entry
  • Associated product(s)
This firmware update V04.02 can be used for SCALANCE M812, M816, M826, M874-x, M876-x and S615 products and replaces the older firmware versions.


You can find additional information on downloading new firmware in the

Configuration Manual 78389151


New functions:

SCALANCE M812-x / M816-x

  • Connection to SINEMA Remote Connect (via KEY-PLUG) 1)

  • PROXY server (OpenVPN client and SINEMA Remote Connect) 1)

  • Support of digital input and output, for example:

    • Tunnel establishment / termination via digital input

    • Setting the digital output when tunnel is established

  • CLI (Command Line Interface)

  • VLAN support

    • Port-based VLANs

    • Tagged VLANs

    • VLAN trunk ports

    • Ingress filter

  • LLDP support

  • Multiple Internal subnet configurable (routable)

  • Masquerading on any VLAN

  • New user administration and password management (multiple users can be defined)

  • Ethernet port configurable (mode, can be switched off individually)

  • Dedicated firewall rules can be configured for each IPSec tunnel

  • Source NAT + NETMAP

  • DHCP server bindings table

  • ANNEX J (on ANNEX B devices)

  • PPPoA

  • DHCP client configurable with deactivated DSL interface

  • Support of static IP addresses at WAN interface

  • Support of static IP addresses at WAN interface (PPPoE)

  • Basic Wizard (specify IP, time settings, DDNS, SINEMA Remote Connect)

1) Only for M816

SCALANCE M826

  • CLI (Command Line Interface)

  • VLAN support

    • Port-based VLANs

    • Tagged VLANs

    • VLAN trunk ports

    • Ingress filter

  • LLDP support

  • Multiple Internal subnet configurable (max. 1 per port, routable)

  • Masquerading on any VLAN

  • New user administration and password management (multiple users can be defined)

  • Ethernet port configurable (mode, can be switched off individually)

  • Dedicated firewall rules can be configured for each IPSec tunnel

  • Source NAT + NETMAP

  • DHCP server bindings table

  • Ring functionality in the SHDSL range

  • Selectable connection profiles ("Reliability", "Standard", "Extended")

    • Improvements in the areas usability and stability

  • Support of up to 19 km (depending on conductor cross-section, quality, age, etc.)

  • Basic Wizard (specify IP, time settings, DDNS, SINEMA Remote Connect)

SCALANCE M874-x / M876-x

  • Basic Wizard (provider list, specify IP, time settings, DDNS, SINEMA Remote Connect)

  • DHCP client configurable with deactivated mobile interface

  • Support of text messages with freely editable text (when sending triggered by digital input)

  • Signal recorder for improved display of the signal strength

  • Display of incoming text messages (SMS) in the log

  • SMS dispatch without APN

SCALANCE S615

  • Basic Wizard (specify default gateway and IP, time settings, DDNS, SINEMA Remote Connect)

Support of affected MLFBs:

Product name

Order number

SCALANCE M812-1 (ANNEX A)

6GK58121AA002AA2

SCALANCE M812-1 (ANNEX B)

6GK58121BA002AA2

SCALANCE M816-1 (ANNEX A)

6GK58161AA002AA2

SCALANCE M816-1 (ANNEX B)

6GK58161BA002AA2

SCALANCE M826-2

6GK58262AB002AB2

SCALANCE M874-2

6GK5874-2AA00-2AA2

SCALANCE M874-3

6GK5874-3AA00-2AA2

SCALANCE M876-3

6GK5876-3AA02-2BA2

SCALANCE M876-3 (ROK)

6GK5876-3AA02-2EA2

SCALANCE M876-4 (EU)

6GK5876-4AA00-2BA2

SCALANCE M876-4 (NAM)

6GK5876-4AA00-2DA2

SCALANCE S615

6GK5615-0AA00-2AA2


Reason for change:

  • PPPoE over external modem

SCALANCE M812 / M816 / M826 / M874-x / M876-x / S615

  • DNS Resolver

  • DDNS for cRSP / SRS

  • Support of VLAN trunk ports

  • Performance improvements regarding 1:1 NAT

  • OpenVPN client

  • In combination with SINEMA Remote Connect:

    • Adjustable auto enrollment interval

Corrections:

SCALANCE M812 / M816 / M826 / M874-x / M876-x / S615

  • Minor improvements

SCALANCE M816 / M826

  • Improvements in handling of saved IP addresses in case of voltage failure

  • Security improvements in the connection check area

  • Stability improvements in the DHCP server area

Security information:

  • This update includes security-related changes. We therefore recommend that you update the firmware.

  • Correction of SSA-301706: GNU C Library Vulnerability in Industrial Products

  • Correction of SSA-342135: Web Vulnerability in SCALANCE M-800 / S615



Third-party software - license conditions and copyright notes

You can find the copyright notes on the third-party software, especially Open Source Software, as well as applicable license conditions for this type of third-party software in the file ReadMe_OSS.

Special note for resellers

The information and the license conditions in the Readme_OSS file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

 Registrierung notwendig  SCALANCE_M_4_2_160816_ReadMe_OSS.html (4,0 MB) 


Description of the download procedure:


For the SCALANCE M81x, SCALANCE M826, SCALANCE M874-x, SCALANCE M876-x and SCALANCE S615 devices, you can download the software free-of-charge as the file "firmware_V04p02p00p00_28p01p01.zip". Double-clicking this file creates the following update file:

- firmware_V04p02p00p00_28p01p01.sfw

You can download the file here:

 Download unterliegt Exportcontrolle  firmware__V04p02p00p00_30p01p01_OSS.zip (19,1 MB)

Note: Software is subject to export restrictions, download only for registered users


Description of the update procedure:

Then open the "System" folder in the Web interface of the corresponding SCALANCE M-800 product and click "Load&Save". In the "Firmware" row, the "firmware_ V04p02p00p00_28p01p01.sfw" file can then be imported by clicking "Load". After the firmware has been successfully loaded into the SCALANCE M-800 / S615 product, you need to perform a restart. You can find additional information on downloading new firmware in the configuration manual 78389151


For SCALANCE M812 / M816

For SCALANCE M81x devices, an additional firmware update of the ADSL firmware is required. Start by updating the device firmware V04.02 first, and then update the ADSL firmware.
You can download the software immediately as free file "firmware_annex_x_enc_sig_trustcenter.sfw". Double-clicking this file creates the following update file:

ANNEX A

- firmware_annex_a_enc_sig_trustcenter.sfw
Here
you can download the file:

 Download unterliegt Exportcontrolle  firmware_annex_a_enc_sig_trustcenter_OSS.zip (8,5 MB)

Note: Software is subject to export restrictions, download only for registered users

ANNEX B:

- firmware_annex_b_enc_sig_trustcenter.sfw
Here
you can download the file.

 Download unterliegt Exportcontrolle  firmware_annex_b_enc_sig_trustcenter_OSS.zip (8,5 MB)

Note: Software is subject to export restrictions, download only for registered users


Third-party software - license conditions and copyright notes

You can find the copyright notes on the third-party software, especially Open Source Software, as well as applicable license conditions for this type of third-party software in the file ReadMe_OSS.

Special note for resellers

The information and the license conditions in the Readme_OSS file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

 Registrierung notwendig  SCALANCE_M_ADSL_V5_2_160908_ReadMe_OSS.html (4,7 MB)


Description of the update procedure:

Then open the "System" folder in the Web interface of the corresponding SCALANCE M-800 product and click "Load&Save". In the "Firmware" row, the "firmware_annex_x_enc_sig_trustcenter.sfw" file can then be imported by clicking "Load". After the firmware has been successfully loaded into the SCALANCE M-800 / S615 product, you need to perform a restart. You can find additional information on downloading new firmware in the configuration manual 78389151


Notes on upgrade of SCALANCE M874 / M876:

  • A firmware update to version V04.02 is only possible with an existing version from V01.02.
    If a version older than V01.02 is installed on the device, you first have to perform a firmware update to this version V01.02. You can find the firmware update to V01.02 here 102780948
    .