×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109741441, Entry date: 09/21/2016
(0)
Rate

Important Licensing Information for PH/IS Software Update from Version 2014 or 2014 SP1 or 2014 SP1 Update 1 to Version 2014 SP2

  • Entry
  • Associated product(s)
If SIMATIC PCS 7 bundle licenses are used, please consider: For updating a PH/IS 2014 or PH/IS 2014 SP1 or PH/IS 2014 SP1 Update 1 to version 2014 SP2, the Process Historian 2014 SP2 DVD (article no. S79220-B6825-P) must be used instead of the SIMATIC PCS 7 V8.2 DVD.

In case of redundant PH installations or when PH and IS are installed together on one machine, so-called bundle licenses exist in the context of SIMATIC PCS 7.

The names of these bundle licenses are „Process Historian Server Redundancy“ (SISLSP7PSR0800, SISLSP7PSR0801) and „Process Historian and Information Server” (SISLSP7PHI0800, SISLSP7PHI0801).

If one of these bundle licenses is used, the following has to be considered:

For updating a PH/IS 2014 or PH/IS 2014 SP1 or PH/IS 2014 SP1 Update 1 to version 2014 SP2, the PCS 7 V8.2 DVD must not be used due to a licensing problem. Instead of that, the Process Historian 2014 SP2 DVD (article no. S79220-B6825-P) must be used.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.