×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109741461, Entry date: 09/30/2016
(10)
Rate

Firmware version V4.2 released for S7-1200 CPUs

  • Entry
  • Associated product(s)
Firmware version V4.2 for S7-1200 CPUs is herewith released for delivery.

Firmware version V4.2 enhances the S7-1200 Hardware version V4  feature set.

New features in the V 4.2 release:

  • Addtional communication capabilities:
    • Time synchronization within central rack between CPU and CM/CP
      (please attend notices below Necessary requirements .... )
    • S7-routing
      (please attend notices below Necessary requirements .... )
    • Autonegotiation
    • Media Redundancy Protocol - higher network availabilty through MRP client support for CPU 1215C and CPU 1217C
    • Support for the 3964R protocol in point-to-point communication
      (please attend notices below Necessary requirements .... )
  • Backup and restore of an S7-1200 CPU
  • Ability to format a SIMATIC memory card from STEP 7
  • Ability to prevent copies from internal load memory to external load memory (SIMATIC memory card)
  • Ability to save trace job measurements to external load memory (SMC)  - Persistent storage of measurements
  • Maximum size of 256KB for unlinked (load memory) data blocks, regardless of CPU model

  • Addtional programming instructions, e.g.:
  • GetInstanceName - Read out name of the block instance
  • D_ACT_DP - Enable/disable PROFINET IO devices
  • PROFIenergy - instructions for energy management
  • Gen_UsrMsg - Generate user diagnostic alarms
  •  CTRL_PTO - Pulse Train Output
  • Data block instructions:
  • DataLogClear - empty data log
  • DataLogDelete - delete dat log
  • CREATE_DB - create data blog
  • ATTR_DB - read data block attribute
  • DELETE_DB  - delete data bloc 

  • Web server enhancements
  • New or improved standard Web page
  • Watch tables - ability to display in engineering system configured watch tables
  • Online backup - easy ability to backup or restore running projects
  • Communication - additional info about communication statistics
  • Program protection - For a quick overview of enabled/disabled security mechanisms  (Know how and Copy protection) in the CPU directly on-site
  • Ability to define user-defined Web page as start page
  • New technology features, e.g.:
  • Enable and disable the HSC with the Gate input
  • Axis control using the TM Pulse module
  • Variable PWM and variable frequencies output  at runtime

  • Addtional failsafe CPUs and support PROFIsafe protocol,see entry109739232 

Affected CPU types and their download links:

 ProductArticle number Download Link FW version 
 CPU 1211 CPU 1211C DC/DC/DC 6ES7 211-1AE40-0XB0 107247170
 CPU 1211C AC/DC/Rly 6ES7 211-1BE40-0XB0 107539610
 CPU 1211C DC/DC/Rly 6ES7 211-1HE40-0XB0 107539825
 CPU 1212 CPU 1212C DC/DC/DC 6ES7 212-1AE40-0XB0 107539748 
 CPU 1212C AC/DC/Rly 6ES7 212-1BE40-0XB0 107539957 
 CPU 1212C DC/DC/Rly 6ES7 212-1HE40-0XB0 107540369 
 CPU 1214 CPU 1214C DC/DC/DC 6ES7 214-1AG40-0XB0 107539750 
 CPU 1214C AC/DC/Rly 6ES7 214-1BG40-0XB0 107540156 
 CPU 1214C DC/DC/Rly 6ES7 214-1HG40-0XB0 107539979 
 CPU 1215 CPU 1215C DC/DC/DC 6ES7 215-1AG40-0XB0 107539980 
 CPU 1215C AC/DC/Rly 6ES7 215-1BG40-0XB0 107540594 
 CPU 1215C DC/DC/Rly 6ES7 215-1HG40-0XB0 107540296 
 CPU 1217 CPU 1217C DC/DC/DC 6ES7 217-1AG40-0XB0 107540595 

Necessary requirements for running the above modules and functionalities

To configure the SIMATIC S7-1200 CPUs version 4.2 and higher you require the Engineering System Step7 with version V14 and higher.

See entry 109740340 

For using the new features

Time synchronization within central rack between CPU and CM/CP
S7-routing

the use of CP firmware at least V 2.1.77 is needed for CP 1242-7 V2, CP 1243-7 LTE, CP 1243-8 IRC , CP 1243-1


The 3964R protocol support for point-to-point communication needs to use firmware version 2.2 at least for CM1241  - see SIOS entry 109741869.


Compatibility and necessary components

SIMATIC Memory Card

A SIMATIC Memory Card can be used optionally for expanding the CPU load memory, loading the application software or for executing a firmware update. 

Compatibility of the hardware and software

Existing SIMATIC S7-1200 CPUs V4 (Article No. 6ES721x-1xx40-0XB0) can be updated to the new CPU firmware 4.2.

An S7-1200 CPU with version 4.2 is replacement compatible with an S7-1200 and firmware version 4.0 and 4.1. This enables the use of an real existing CPU with firmware version 4.2 with an engineered V4.0 or V4.1 based on an existing TIA portal V13 or V13 Service Pack 1 project. The new firmware features can't used in that case.

Further information:

Internet Web page S7-1200  
System manual "SIMATIC S7-1200 Programmable controller", Edition 09/2016 109741593 
Documentation portal for SIMATIC Controller Link 
Programming Guidelines for S7-1200 und S7-1500 81318674 
SIMATIC S7-1200 / S7-1500 Comparison list for programming languages based on the international mnemonics 86630375 
Product note Firmware version 4.1 106200276 
Product note Firmware version 4.0 86567043 

 



Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.