×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109741643, Entry date: 02/24/2017
(0)
Rate

Power losses / contact resistance for 3SB1 / 3SB2 / 3SB3 / 3SE3 / 3SE5 / 3SU1

  • Entry
  • Associated product(s)
This entry contains information about contact resistance for 3SB1 / 3SB2 / 3SB3 / 3SE3 / 3SE5 / 3SU1 units

QUESTION:

How high is the contact resistance for 3SB1 / 3SB2 / 3SB3 / 3SE3 / 3SE5 / 3SU1 units?

ANSWER:

For as-new 3SB1 / 3SB2 / 3SB3 / 3SE3 / 3SE5 / 3SU1 devices, contact resistance is, on average, 20 milliohms, however, contact resistances of up to 100 milliohms are permissible.

Currents of 10 mA are typical in the control circuit when connected to a PLC.
At 10 mA, power losses are only 0.002 mW (P = I² * R).

Here are some general details regarding power loss:

- Contact power loss is proportional to the current load
- The total power loss is the sum of the power loss of the contacts + power loss of the clamping point + power loss of the supply cable
- The power loss of the contact is largely determined by its condition (e.g. oxide layers).

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.