×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109741912, Entry date: 05/24/2017
(25)
Rate

SINAMICS Startdrive V13 SP2

  • Entry
  • Associated product(s)
You can find the Startdrive version V13 SP2

You can find the latest Startdrive version here: 68034568


SINAMICS Startdrive V13 SP2

OSS note on SINAMICS Startdrive V13 SP2

Third-party software - license conditions and copyright notes
You can find the copyright notes on the third-party software, especially Open Source Software, as well as applicable license conditions for this type of third-party software in the following file:

 Registrierung notwendig  Readme_OSS_All_Languages.htm (1,1 MB)

Special note for resellers
The information and the license conditions in the ReadMe_OSS.htm file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

OSS Source Code
The source code files are part of the download package and can be downloaded here separately:

 Registrierung notwendig  OpenSourceSoftware_SDR_V13SP2.zip (723,3 KB)


SINAMICS Startdrive V13 SP2 Option Package for SIMATIC STEP 7 V13 SP2

Here you can find the Startdrive commissioning tool for the SINAMICS G120 drive Family.

SINAMICS Startdrive V13 SP2 options package

SINAMICS Startdrive V13 SP2 options package for SIMATIC STEP 7 V13 SP2 

The option package is to be used if TIA Portal V13 SP2 is already installed.  STEP 7 needs to be installed first.

Associated sales information you can find here 109746258 

 Registrierung notwendig  Startdrive_Optional_V13_SP2.zip (1,6 GB)

SHA-256 checksum:

34FD69C59519032F6B0BE4E362B0CCDAFAB6BDEA2B860B7FF33E4A36C2BB8565

SINAMICS Startdrive V13 SP2 Update 1
Associated sales information you can find here 109747522

Update 1 has been withdrawn.

SINAMICS Startdrive V13 SP2 Update 2

Associated sales information 109749514 

 Registrierung notwendig  SINAMICS_Startdrive_V13SP2_UPD2.001 (650,0 MB)

 Registrierung notwendig  SINAMICS_Startdrive_V13SP2_UPD2.002 (650,0 MB)

 Registrierung notwendig  SINAMICS_Startdrive_V13SP2_UPD2.003 (52,8 MB)

 Registrierung notwendig  SINAMICS_Startdrive_V13SP2_UPD2.exe (2,7 MB)

SHA-256 checksum:  Registrierung notwendig  SINAMICS_Startdrive_V13_SP2_Update_2.txt (1 KB) 

Information regarding SHA-256 checksum 109483101 

Use of SINAMICS Startdrive is free of charge and does not require a license key to be entered.

Startdrive supports the languages German, English, French, Spanish, Italian and Chinese (simplified).

How to install Startdrive V13 SP2:

  1. Download the attached ZIP file
  2. Unpack the ZIP file into a target directory on your hard disk. Pleae make sure that no spaces are contained in the entire path name of this target directory.
  3. After unpacking there must be the file "Startdrive_Optional_V13_SP2.exe" in the directory.
  4. Launch Startdrive using Startdrive_Optional_V13_SP2.exe.

 

SINAMICS Startdrive V13 SP2 Standalone

Here you can find the Startdrive commissioning tool for the SINAMICS G120 drive Family.

SINAMICS Startdrive V13 SP2 Standalone

SINAMICS Startdrive V13 SP2 Standalone   

The standalone package should be used when STEP 7 V13 SP2 has not been installed.
Associated sales information you can find here 109746258 

 Registrierung notwendig  Startdrive_Standalone_V13_SP2.zip (2,1 GB) 

SHA-256-checksum::

02DB500F594262380604F98E70F33CB261538377DBD60E0C3C429C4AC6F167A7

Note
The simultaneous installation and operation of the STEP 7 and Startdrive Standalone variants on one PC/PG is supported as of Version V13, whereby the versions must be the same.
For example, STEP 7 V13 and Startdrive Standalone V13 or STEP 7 V13 SP2 and Startdrive Standalone V13 SP2.
With such variants, there are no differences or restrictions in the functionality (integration, operation, etc.) compared to the STEP 7 and Startdrive option package variants.

Use of SINAMICS Startdrive is free of charge and does not require a license key to be entered.

Startdrive supports the languages German, English, French, Spanish, Italian and Chinese (simplified).

How to install Startdrive V13 SP2:

  1. Download the attached ZIP file
  2. Unpack the ZIP file into a target directory on your hard disk. Pleae make sure that no spaces are contained in the entire path name of this target directory.
  3. After unpacking there must be the file "Startdrive_Standalone_V13_SP1.exe" in the directory.
  4. Launch Startdrive using Startdrive_Standalone_V13_SP1.exe.


Predecessor version:

SINAMICS Startdrive V13 SP1

For customers who do not want to upgrade to the Startdrive V13 SP2 version, the predecessor version of Startdrive V13 SP1 is offered for a transitional period.
If Startdrive V13 SP1 is still to be used and is not the standalone version, the TIA environment shall not be upgraded to V13 SP2.

Unlike Startdrive V13 SP2, the SINAMICS firmware versions V4.7 SP3 and V4.7 SP6 are not included in Startdrive V13 SP1 and must be installed using Hardware Support Packages.


SINAMICS Startdrive V13 SP1 Option Package for SIMATIC STEP 7 V13 SP1

Here you can find the Startdrive commissioning tool for the SINAMICS G120 drive Family.

SINAMICS Startdrive V13 SP1 options package

SINAMICS Startdrive V13 SP1 options package for SIMATIC STEP 7 V13 SP1

The option package is to be used if TIA Portal V13 SP1 is already installed.  STEP 7 needs to be installed first.

Associated sales information you can find here 107657741 

 Registrierung notwendig  startdrive_optional_v13_sp1.zip (939,1 MB)

SHA-256-checksum:

C87EF809F54F231D482828B6019E8C806174C8F668939F9C2E07FF396793984

SINAMICS Startdrive V13 SP1 Update 1

Associated sales information you can find here 109476628 

 Registrierung notwendig  V13_SP1_Update1.zip (855,8 MB)

SHA-256-checksum: 

EA4C9E47DA28D09259286AD08473129B136E9C395DBA1B72DE114806F6147F80
SINAMICS Startdrive V13 SP1 Update 3

Associated sales information you can find here 109481727  

 Registrierung notwendig  Startdrive_V13_SP1_Upd3.zip (1,2 GB) 

SHA-256-checksum: 

DA27E064DCE6D7EDB22B01D5B7622B76945EF249A2A65F8FC7A44E543017BA73

Use of SINAMICS Startdrive is free of charge and does not require a license key to be entered.

Startdrive supports the languages German, English, French, Spanish, Italian and Chinese (simplified).

How to install Startdrive V13 SP1:

  1. Download the attached ZIP file
  2. Unpack the ZIP file into a target directory on your hard disk. Pleae make sure that no spaces are contained in the entire path name of this target directory.
  3. After unpacking there must be the file "Startdrive_Optional_V13_SP1.exe" in the directory.
  4. Launch Startdrive using Startdrive_Optional_V13_SP1.exe.

Procedure for the installation of Startdrive V13 SP1 Update 1/3:

  1. Download the attached ZIP file.
  2. Unpack the ZIP file into a target directory on your hard disk. Please ensure that there are no spaces in the entire path name of this target directory. 
  3. After unpacking, the file "Start.exe" must be in the directory.
  4. Start installation by calling the "Start.exe". 


SINAMICS Startdrive V13 SP1 Standalone

Here you can find the Startdrive commissioning tool for the SINAMICS G120 drive Family.

SINAMICS Startdrive V13 SP1 Standalone

SINAMICS Startdrive V13 SP1 Standalone
The standalone package should be used when STEP 7 V13 SP1 has not been installed.
Associated sales information you can find here 107657741  

 Registrierung notwendig  startdrive_standalone_v13_sp1.zip (1,5 GB) 

SHA-256-checksum: 

5A22A4034F313B25AAFA252F2C5B81B2E0CF4B353865EE39EE73A6910DD8DEB1

SINAMICS Startdrive V13 SP1 Update 1

Associated sales information you can find here 109476628 

 Registrierung notwendig  V13_SP1_Update1.zip (855,8 MB)

SHA-256-checksum: 

EA4C9E47DA28D09259286AD08473129B136E9C395DBA1B72DE114806F6147F80
SINAMICS Startdrive V13 SP1 Update 3

Associated sales information you can find here 109481727  

 Registrierung notwendig  Startdrive_V13_SP1_Upd3.zip (1,2 GB) 

SHA-256-checksum: 

DA27E064DCE6D7EDB22B01D5B7622B76945EF249A2A65F8FC7A44E543017BA73
Note
The simultaneous installation and operation of the STEP 7 and Startdrive Standalone variants on one PC/PG is supported as of Version V13, whereby the versions must be the same.
For example, STEP 7 V13 and Startdrive Standalone V13 or STEP 7 V13 SP1 and Startdrive Standalone V13 SP1.
With such variants, there are no differences or restrictions in the functionality (integration, operation, etc.) compared to the STEP 7 and Startdrive option package variants.

Use of SINAMICS Startdrive is free of charge and does not require a license key to be entered.

Startdrive supports the languages German, English, French, Spanish, Italian and Chinese (simplified).

How to install Startdrive V13 SP1:

  1. Download the attached ZIP file
  2. Unpack the ZIP file into a target directory on your hard disk. Pleae make sure that no spaces are contained in the entire path name of this target directory.
  3. After unpacking there must be the file "Startdrive_Standalone_V13_SP1.exe" in the directory.
  4. Launch Startdrive using Startdrive_Standalone_V13_SP1.exe. 

Procedure for the installation of Startdrive V13 SP1 Update 1/3:

  1. Download the attached ZIP file.
  2. Unpack the ZIP file into a target directory on your hard disk. Please ensure that there are no spaces in the entire path name of this target directory. 
  3. After unpacking, the file "Start.exe" must be in the directory.
  4. Start installation by calling the "Start.exe".


SINAMICS Startdrive V13 SP1 Support Package for SINAMICS Firmware V4.7 SP6

Here you can find the SINAMICS Startdrive V13 SP1 Support Package for SINAMCIS Firmware V4.7 SP6.

SINAMICS Startdrive V13 SP1 Support Package Firmware V4.7 SP6

SINAMICS Startdrive V13 SP1 Support Package for SINAMICS Firmware V4.7 SP6

Associated sales information you can find here 109482758 

 Registrierung notwendig  Startdrive_V13_SP1_HSP_FW_4_7_SP6.zip (358,7 MB)

SHA-256-checksum:

0BB60F45E1E0409A9064E4375E62AAA0B011BBCC34D6A895F05BF791F81FBDBC

Installation notes SINAMICS Startdrive V13 SP1 Support Package for SINAMICS Firmware V4.7 SP6.
On 54163658 you will find the procedure for updating the hardware catalog of your Startdrive (TIA Portal) installation with this download. The support package for the SINAMICS firmware version 4.7 SP6 can only be installed if Startdrive V13 SP1 has already been installed. If Startdrive V13 SP1 is reinstalled, the Support Package must also be reinstalled.


SINAMICS Startdrive V13 SP1 Support Package for SINAMICS Firmware V4.7 SP3

Here you can find the SINAMICS Startdrive V13 SP1 Support Package for SINAMCIS Firmware V4.7 SP3.

SINAMICS Startdrive V13 SP1 Support Package Firmware V4.7 SP3

SINAMICS Startdrive V13 SP1 Support Package for SINAMICS Firmware V4.7 SP3

Associated sales information you can find here 109476629 

 Registrierung notwendig  Startdrive_V13_SP1_HSP_FW_4_7_SP3.zip (362,3 MB)

SHA-256-checksum:

57C79A36B7E404696B6CDB209505CB67AE012C038EFCEE36758C0BCD3FE48081

Installation notes SINAMICS Startdrive V13 SP1 Support Package for SINAMICS Firmware V4.7 SP3.
On 54163658 you will find the procedure for updating the hardware catalog of your Startdrive (TIA Portal) installation with this download. The support package for the SINAMICS firmware version 4.7 SP6 can only be installed if Startdrive V13 SP1 has already been installed. If Startdrive V13 SP1 is reinstalled, the Support Package must also be reinstalled.


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit