×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109742154, Entry date: 02/07/2019
(15)
Rate

SIMATIC PCS 7 Plant Automation Accelerator (PAA) using a practical example

  • Entry
  • Associated product(s)
SIMATIC PCS 7 Plant Automation Accelerator (PAA) proposes the digital bridge between plant planning and process control system SIMATIC PCS 7. With this application example, you will learn about the basic functions and advantages of SIMATIC PCS 7 Plant Automation Accelerator using a standard workflow.



Objective of this application example
This application example is a "best practice" example and shows you the basic functions and benefits of the SIMATIC PCS 7 Plant Automation Accelerator (PAA) software solution by means of a sample project.

PAA is used primarily in the detail engineering phase of plant planning.
In this planning phase, there are a variety of requirements to improve the conventional planning process of an installation, save time, reduce costs, and conserve resources.
The following challenges and questions result from this:

  • There may be errors and inconsistencies, since different tools are used and the multiplicity of interfaces increase the error potential.
  • Different data bases are used.
  • The traceability of changes must be ensured.
  • Data must be entered once and be able to be used again.
  • How can projects be more efficiently planned and documented?
  • How can the project quality be improved?
  • How can project flexibility and duration be improved?
  • How can costs be reduced?

This application sample provides an initial insight into how you can implement the requirements and issues shown here, using the SIMATIC PCS 7 Plant Automation Accelerator software solution.
 


Documentation and example project data as of PAA V2.1 and SIMATIC PCS 7 V9.0
Documentation and example project data as of PAA V1.0.2 and SIMATIC PCS 7 V8.2
  PAA Application example documentation (15,0 MB)
 Registrierung notwendig  PAA Application example project data (259,5 MB)

Last change
Update of the application example to PAA V2.1 and SIMATIC PCS 7 V9.0

Further Information
Application example - Controlled plant engineering from the outset with COMOS FEED
Application example - Fast and easy generation of Piping and Instrumentation Diagrams with COMOS P&ID using a practical example
Application example - Integrated Engineering with COMOS and SIMATIC PCS 7 using a practical example
Application example - Automated creation of the SIMIT simulation model with COMOS planning and engineering data
Video - Integrated Engineering on the basis of COMOS with SIMATIC PCS 7 and SIMIT Simulation (Video)
Media System - COMOS
 
More help and useful information about this topic you can get via the COMOS and PCS 7 topic page:
www.siemens.com/onlinesupport/comos
www.siemens.com/onlinesupport/pcs7
 

Additional keywords
PAA, PAA Best practice, PAA Application, PAA Getting Started, PAA Training, Dígitalization, Process Automation

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.