×
Siemens Industry Online Support
Siemens AG
Type bericht: Productmededeling ID van bericht: 109742307, Datum bericht: 10/21/2020
(6)
Beoordelen

Requesting a test rack license for SINUMERIK 828D/SINUMERIK 840D sl

  • Bericht
  • Heeft betrekking op product(en)
The test rack license was developed for testing and presentation purposes. Using this license, the NC start lock is withdrawn, and all options can be freely tested.

In order to obtain it, customers must have a Siemens CF card with licensed CNC software, and the signed "Confirmation Letter Test Racks" must be available for the SINUMERIK license management.
The test rack license is available for SINUMERIK 840D sl from SW 4.6 - and for SINUMERIK 828D from SW 4.7 SP3.


demonstration machine/test rack

Procedure

  • The Siemens sales partner for the customer downloads the "Confirmation Letter Test Racks".
  • This confirmation letter is used to confirm that the requested license will be exclusively used for test purposes only.
  • The confirmation letter is completed and signed by the Siemens sales person and the customer (see below: Completing the test rack confirmation letter).
  • The completed confirmation letter is returned to the specified fax/mail address.
  • The test rack licenses are generated by the license management, and assigned to the specified CF card.
  • The customer contact person then receives an email with the .alm file for the new license key.
  • This .alm file can be read into the machine from the USB stick.
  • The NC start interlocking is withdrawn, and all options can be freely tested.
  • Alarm 8086 "Test and demonstration machine" is displayed on the machine.

Note

  • If a trial period was started before the test rack is licensed, the trial period continues to run until the current trial period has expired.
  • After all of the trial periods expire, the test rack license cannot withdraw the NC start interlock.
  • The test rack license is issued but can be retracted. This means that Siemens has the right to withdraw the license.

Completing the "Confirmation Letter Test Racks"

  • The Siemens sales person for the customer, including department name and ORG-ID, are entered under "sales person".
  • The company name of the customer including ORG-ID is entered under "Customer".
  • The machine identifier of the test rack is entered under "Test rack name". The required machine identifier must be entered here if the test rack still does not have a machine identifier.
  • The serial number of the CF card, which should be assigned to the test rack license, is entered under "Hardware serial number of the CF card" (it is printed on the CF card).
  • The customer confirms the order with his signature (an electronic signature is not permissible!) under "Confirm"
  • The customer’s employee who is responsible for the test rack is noted under "Mail address (alm. file)" and "Customer contact person, telephone". The new license key for the test rack is sent to the customer specified here.

Confirmation Letter Test Rack for SINUMERIK 828D

Confirmation_letter_test_racks_828D_SW4.doc (29.0 KB)

Confirmation Letter Test Rack for SINUMERIK 840D sl

Confirmation_letter_test_racks_840D_sl.doc (29.0 KB)

Return of TestRack license

The TestRack license is taken back via the following contact

Contact: licensemanagementmts.industry@siemens.com 


Nota's in verband met security
Ter bescherming van technische infrastructuur, systemen, machines en netwerken tegen digitale dreigingen is het noodzakelijk om een alomvattend 'IT Security' concept te implementeren (en continu te handhaven) dat overeenkomt met de huidige stand van de techniek. De producten en oplossingen van Siemens vormen slechts een klein deel van een dergelijk concept. Meer informatie over 'Cyber Security' vindt u op
https://www.siemens.com/cybersecurity#Ouraspiration.
Bericht beoordelen
geen beoordeling
Verzoeken en feedback
Wat wilt u doen?
Opmerking: de feedback heeft altijd betrekking op het actuele artikel/product. Uw bericht wordt naar de technische redacteurs van de Online Support gestuurd. We zullen binnen enkele dagen antwoorden als uw feedback dat vereist. Als we geen vragen meer hebben, zullen we geen antwoord meer sturen.