×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109742334, Entry date: 12/21/2016
(22)
Rate

SIMOTION SCOUT, SCOUT Stand-alone and SCOUT TIA V4.5 HF1

  • Entry
  • Associated product(s)
Download of SIMOTION SCOUT, SCOUT Stand-alone and SCOUT TIA V4.5 HF1

General Information

Attached you can find hotfix 11 for the engineering systems SIMOTION SCOUT, SCOUT Stand-alone and SCOUT TIA V4.5 HF 1.
Three different installation packages are offered as download:
 

Installation package

Designation

Directories

Content

Package 1

SCOUT

V4.5 + HF1

(complete setup)

VOL1
SCOUT V4.5 + HF1
Addon
CamTool
HSP..TM_Timer_...
InstData
SSP_...
SIMOTION complete setup
SCOUT V4.5 + HF1
200SP Timer DIDQ
SSPs for SINAMICS

VOL2

SCOUT V4.5 + HF1

Documentation

Documentation
STEP7_V55_SP4_HF11
Utilities_Applications
 
SIMOTION V4.5 Documentation
STEP7 V5.5 SP4 HF11 (required for the installation)

 

VOL3

SCOUT TIA V4.5 + HF1

ScoutTia
MigTool
 
SIMOTION complete setup
SCOUT TIA V4.5 + HF1
(incl. CamTool V3.0 SP3 HF2)
SCOUT Migrations-Tool Plug-In V4.5 + HF1
 

Package 2:

SCOUT Stand-alone 

V4.5 + HF1

(complete setup)

 

VOL1
SCOUT Stand-alone
 

V4.5 + HF1

SC
Addon
CamTool
HSP..TM_Timer_...
InstData
SSP_...

SIMOTION complete setup
SCOUT Stand-alone V4.5 HF1
 

VOL2

SCOUT Stand-alone
V4.5 + HF1
Documentation

Documentation
Utilities_Applications
 
SIMOTION V4.5 Documentation

Package 3:

SCOUT TIA

V4.5 + HF1

(TIA Portal Client-Setup)

SCOUT TIA V4.5 + HF1

ScoutTia
MigTool 

SIMOTION complete setup
SCOUT TIA V4.5 HF1
(incl. CamTool V3.0 SP3 HF2)
SCOUT Migrations-T
ool Plug-In V4.5 HF1

 Requirements for the installation:

  • For SCOUT, SIMATIC STEP 7 V5.5 SP4 HF11 installed on the engineering computer. This SIMATIC Hotfix is in the directory VOL1.  The SIMOTION SCOUT Version V4.5 HF1 is a complete installation of SCOUT.
  • For SCOUT TIA, TIA Portal Framework V14 installed on the engineering computer (SCOUT TIA is a TIA Portal client setup). We recommend that you use the latest update of TIA Portal V14.

Further information about V4.5 HF1 is available in the delivery release notice 109742328 .


Third-party software - Licensing terms and copyright information

You can find the copyright information for third-party software contained in this product, particularly open source software, as well as applicable licensing terms of such third-party software in the Read_OSS file.
Special information for resellers:

The information and the license terms in the Read_OSS file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

 Registrierung notwendigRead_OSS.ZIP (1,4 MB)

Availability of Source Code
Certain license conditions of third-party software components used in this product may require Siemens to provide you with the source code and additional information for such components. In most cases, Siemens provides this information on or with the device. In case Siemens is technically unable to do so, you may request a copy of this OSS source code against payment of shipping and handling charges. Please send your request to the address provided at the end of this section.

Siemens AG 
Digital Factory
Customer Services DF&PD
DF CS SD CCC TS
Gleiwitzer Str. 555
90475 Nuernberg, Germany
Internet: http://www.siemens.com/automation/support-request
Tel.: +49 911 895 7222
Email: support.automation@siemens.com
 


Notes on the installation packages

The installation packages are divided into multiple files. First download all the parts into the same folder and run the file with the .exe extension. Select the root-directory of one of your hard disks to extract the setup files.The parts are then joined up and you can execute the setup.

 

Installation package 1: SIMOTION SCOUT V4.5 HF1

 Registrierung notwendig  SCOUT_V4_5_0_1.exe (2,6 MB) 
 Registrierung notwendig  SCOUT_V4_5_0_1.001 (667,6 MB) 
 Registrierung notwendig  SCOUT_V4_5_0_1.002 (667,6 MB) 
 Registrierung notwendig  SCOUT_V4_5_0_1.003 (667,6 MB) 
 Registrierung notwendig  SCOUT_V4_5_0_1.004 (667,6 MB) 
 Registrierung notwendig  SCOUT_V4_5_0_1.005 (667,6 MB) 
 Registrierung notwendig  SCOUT_V4_5_0_1.006 (667,6 MB) 
 Registrierung notwendig  SCOUT_V4_5_0_1.007 (667,6 MB) 
 Registrierung notwendig  SCOUT_V4_5_0_1.008 (667,6 MB) 
 Registrierung notwendig  SCOUT_V4_5_0_1.009 (667,6 MB) 
 Registrierung notwendig  SCOUT_V4_5_0_1.010 (667,6 MB) 
 Registrierung notwendig  SCOUT_V4_5_0_1.011 (667,6 MB) 
 Registrierung notwendig  SCOUT_V4_5_0_1.012 (667,6 MB) 
 Registrierung notwendig  SCOUT_V4_5_0_1.013 (667,6 MB) 
 Registrierung notwendig  SCOUT_V4_5_0_1.014 (667,6 MB) 
 Registrierung notwendig  SCOUT_V4_5_0_1.015 (667,6 MB) 
 Registrierung notwendig  SCOUT_V4_5_0_1.016 (594,3 MB) 


Installation package 2: SIMOTION SCOUT Stand-alone V4.5 HF1

Note
For the on-line help the Microsoft KB917607 update is required. If KB917607 is not installed, it is automatically downloaded via an Internet connection and installed. If there is no internet connection available during the installation, you must install KB917607 manually bevor you start setup.exe.
You can download KB917607 at  https://support.microsoft.com/en-us/kb/917607 

 Registrierung notwendig  SCOUT_SA_V4_5_0_1.exe (2,6 MB)
 Registrierung notwendig  SCOUT_SA_V4_5_0_1.001 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V4_5_0_1.002 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V4_5_0_1.003 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V4_5_0_1.004 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V4_5_0_1.005 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V4_5_0_1.006 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V4_5_0_1.007 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V4_5_0_1.008 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V4_5_0_1.009 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V4_5_0_1.010 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V4_5_0_1.011 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V4_5_0_1.012 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V4_5_0_1.013 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V4_5_0_1.014 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V4_5_0_1.015 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V4_5_0_1.016 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V4_5_0_1.017 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V4_5_0_1.018 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V4_5_0_1.019 (165,1 MB)


Installation package 3: SIMOTION SCOUT TIA V4.5 HF1

 Registrierung notwendig  SCOUT_TIA_V4_5_0_1.exe (2,6 MB)
 Registrierung notwendig  SCOUT_TIA_V4_5_0_1.001 (667,6 MB)
 Registrierung notwendig  SCOUT_TIA_V4_5_0_1.002 (667,6 MB)
 Registrierung notwendig  SCOUT_TIA_V4_5_0_1.003 (667,6 MB)
 Registrierung notwendig  SCOUT_TIA_V4_5_0_1.004 (181,3 MB)

Note
If you use SCOUT TIA V4.5 HF1 and SCOUT V4.4 in one partition, see entry ID 109745779 


Further downloads

The following downloads are also available as a single download from the Internet Product Support pages. The components are also includes in the download of SIMOTION SCOUT and SCOUT Stand-alone (= installation package 1 and 2).

  • SIMOTION C kernel/firmware V4.5 HF1, see 31263919
  • SIMOTION D kernel/firmware V4.5 HF1, see 31045047
  • SIMOTION  Firmware Support Package (FWSP) for device update tool, see 33119786 
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.