×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 109743172, Entry date: 02/24/2017
(0)
Rate

3SU1 definition of degree of protection IP69K - IP69

  • Entry
  • Associated product(s)
This entry contains details on the definition of degree of protection IP69K - IP69

QUESTION:

What does degree of protection IP69K mean?
What is the difference between IP69 and IP69K?



ANSWER:

What does degree of protection IP69K mean for 3SU1 units?



Degree of protection IP69K was developed for high-pressure jet cleaning at high temperatures. "6" stands for protection against the ingress of dust, while "9" signifies protection against jets during close-range high-pressure cleaning.
Degree of protection IP69K was introduced in 1993 and is based on the
standard DIN 40050-9. Originally, this degree of protection was developed for automobiles for protecting against the ingress of foreign bodies, such as dust and dirt, and hot water jets.
In the latest version of the standard IEC 60529, only degree of protection IP69 is mentioned (IP69K = IP69).


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.