×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 109743243, Entry date: 03/09/2017
(0)
Rate

Mounting of 3SU1 blind flanges

  • Entry
  • Associated product(s)
This article contains information on the mounting of 3SU1 blind flanges.

QUESTION:

How are 3SU1 blind flanges mounted? Is a holder required for this?



ANSWER:

3SU1 blind flanges are mounted like control elements with holder (to be ordered separately). This provides the advantage that the unit can be prewired, which is important for the option design if a function shall initially not be connected to the outside.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.