×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109743596, Entry date: 12/02/2016
(1)
Rate

Type of protection "Non-sparking equipment – Ex nA"

  • Entry
  • Associated product(s)

The new edition of IEC/EN 60079-7 published in 2015 introduced the future successor of the "Ex nA" type of protection. "Ex nA" has changed its name to "Ex ec". In technical terms, both types of protection are identical.

How long will the designation "Ex nA" continue to apply? 

There is still no expiration date for the "Ex nA" standard (IEC/EN 60079-15:2010). This is why both types of protection are admissible on the market in parallel. However, we anticipate that the "Ex nA" type of protection will be removed from the standard in the next two years. 

From when on will it be obligatory to mark new devices with "Ex ec"? 

After the expiration period of IEC/EN 60079-15:2010, all new devices put into circulation will have to be marked with "Ex ec". We expect the date of expiration will be in about four years from now. 

When will the "Ex ec" designation be coming for our PD PA PI field devices? 

The changeover from "Ex nA" to "Ex ec" has already begun. All devices will be changed over successively in the years to come. The change will be visible in labeling, documentation and the affected certificates. 

May I operate "Ex nA" and "Ex ec" equipment together? 

Yes. "Ex ec" was introduced explicitly as the successor for the "Ex nA" type of protection and has been confirmed as being technically identical. 

This information concerns the following products: all products from PD PA PI

PD PA PI PRM PIP
Dr. Jürgen Ficker
Tel: +49 721 595 3522
E-Mail: juergen.ficker@siemens.com

Download   info (62,2 KB)

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.