×
Siemens Industry Online Support
Siemens AG
Tipo de post: Notificação de produto ID do post: 109743711, Data do post: 09.12.2016
(0)
Avaliar

Sales/Delivery Release of SIMATIC NET DVD V14

  • Post
  • Está relacionado com produto(s)
The SIMATIC NET PC software products (SOFTNET-IE S7 Lean, HARDNET-IE S7 REDCONNECT, etc.) associated with the SIMATIC NET DVD V14 are released for sale and delivery effective immediately. In the process, the product portfolio has been expanded and upgraded by different functionalities and operating systems. The SIMATIC NET DVD V14 will immediately replace the SIMATIC NET DVD V13 because its functions are compatible.


SIMATIC NET CD V7.1 (including SP6) also remains available / can still be ordered for the operating system environments of the Windows XP and the Server 2003 family.

Note that the delivery form OSD (Online Software Delivery) has been offered for some products as of SIMATIC NET V12.
You can find additional information and ordering data in section 2.4.


1. Product description

The products of the SIMATIC NET DVD V14 support the following operating systems:

  • Windows 7 Ultimate, Professional SP1 (32-bit and 64-bit)

  • Windows 8.1 Pro (64-bit)

  • Windows Server 2008 R2 SP1 (64-bit)

  • Windows Server 2012 R2 (64-bit)

  • Windows 10 Pro, Enterprise (64-bit) as of version 1607

You can find the detailed approved operating systems for the individual products in the Readme in the section "Operating systems".

An important highlight of the SIMATIC NET PC software V14 is the new product SOFTNET-IE S7 Extended for using the S7 protocol with up to 255 stations (S7-300 and S7-400 stations) or the S7opt protocol with up to 512 stations (S7-1200 (V4.0 and higher) and S7-1500 stations). In addition, functions have been added in the area of the OPC UA, such as Alarm&Condition and support of UserDefinedTypes (UDT) and multi-instance DBs with access to optimized DBs for S7-1200 V 4.0 and higher / S7-1500. Please also see the notes and information in the SIMATIC NET PC Software V14 Installation Manualand in the Readme.

Liesmich.htm (619.3 KB)

Readme.htm (664.0 KB)


Upgrade of the SIMATIC NET PC software by the following new functionalities:

a) New product SOFTNET-IE S7 Extended

The SOFTNET-IE S7 Extended product expands scaling based on the existing product SOFTNET-IE S7. This enables communication via the S7 protocol with up to 255 stations (S7-300 and S7-400 stations) or by using the S7opt protocol with up to 512 stations (S7-1200 (V4.0 and higher) and S7-1500 stations). Please note that the configuration with STEP7 is limited to 207 connections per application (e.g. OPC Server) but that up to 512 connections are available with COML-S7.

b) Faster connection monitoring for HARDNET-IE S7 REDCONNECT
As of SIMATIC NET DVD V13 the CP 1623 was adapted to the firmware of the CP 1628. This means "fast H-Alive" for faster connection monitoring for HARDNET-IE S7 REDCONNECT is now also possible with CP 1623. More specific monitoring times are available in the quantity framework document (Entry: http://support.automation.siemens.com/WW/view/en/15227599)

c) Alarm & Condition for S7-1500
Alarm & Condition is now supported for the S7OPT OPC UA server. This means you have the option to configure up to 1000 program alarms for Industrial Ethernet.

d) Support of UserDefinedTypes and multi-instance DBs
UDTs and multi-instance DBs are supported with access to optimized DBs for S7-1200 (V4.0 and higher) and S7-1500 stations.

e) Configuration change to STEP7 Professional V14
STEP7 Professional V14 is included in the delivery as a configuration tool and can be used in two ways:

  • For configuring the PC CPs (without additional license)

  • For configuring all modules (for two weeks as part of the TRIAL license)

f) Support of VMware vSphere ESXi V6.0
You can find additional information in the Readme.

g) Support of VMware Workstation V12.5
for test and simulation, may not be used in productive operation

f) Support of Microsoft Hyper-V
You can find additional information in the Readme.

Please note:
The products SOFTNET-PB S7 V14, SOFTNET-PB DP V14 and SOFTNET-PB DP slave V14 have not been approved for the modules CP 5611 A2 and CP 5621. The modules CP 5612, CP 5622 and CP 5711 are released.

The SOFTNET PROFIBUS products V8.1 and V8.2 are still released and available for delivery with the existing scope of functions. There is currently no substitution with V14.

The SOFTNET-IE S7 PG product has been discontinued. All functions are covered by the less expensive product SOFTNET-IE S7 Lean.

The SOFTNET-IE PN IO product is not released in the environment of the SIMATIC NET DVD V14.

1.1 Revision history
A detailed revision history of the SIMATIC NET PC software is available here.

Revision history_20150127.pdf (57.1 KB)

1.2 Supported embedded systems
You can find configurations that have been released for operation in combination with embedded operating system environments and the SIMATIC NET PC software in the following entry: 63097623

Note:
Compared to this general delivery release, the release information of the SIMATIC NET DVD V14 for embedded systems will be available somewhat later.


2. Ordering data

The SIMATIC NET DVD V14 is included with the following products. Please note the entries in the Readme for the specific product.

2.1 PROFIBUS Software Products V14

Product

Version

MLFB

SOFTNET-PB S7

V14

6GK1704-5CW14-0AA0

SOFTNET-PB DP

V14

6GK1704-5DW14-0AA0

SOFTNET-PB DP slave

V14

6GK1704-5SW14-0AA0

HARDNET-PB S7

V14

6GK1713-5CB14-0AA0

HARDNET-PB DP

V14

6GK1713-5DB14-0AA0

HARDNET-PB CP56x3 driver software / DP Base interface

V14

-without MLFB-
supplied with CP
(MLFBs of the CPs:
6GK1561-3AA01,
6GK1561-4AA01,
6GK1561-3AA02,
6GK1561-4AA02,
6GK1562-3AA00,
6GK1562-4AA00)

2.2 INDUSTRIAL ETHERNET Software Products V14

Product

Version

MLFB

HARDNET-IE S7

V14

6GK1716-1CB14-0AA0

HARDNET-IE S7 REDCONNECT

V14

6GK1716-0HB14-0AA0

HARDNET-IE S7 REDCONNECT Power Pack

V14

6GK1716-0HB14-0AC0

SOFTNET-IE S7 REDCONNECT

V14

6GK1704-0HB14-0AA0

SOFTNET-IE S7

V14

6GK1704-1CW14-0AA0

SOFTNET-IE S7 Lean

V14

6GK1704-1LW14-0AA0

SOFTNET-IE S7 Extended

V14

6GK1704-1BW14-0AA0

SOFTNET-IE RNA

V14

6GK1711-1EW14-0AA0

2.3 SNMP Software Products V14

Product

Version

MLFB

Comment

SNMP OPC Server Basic

V14

6GK1706-1NW14-0AA0

Administration of up to 20 IP addresses

SNMP OPC Server Extended

V14

6GK1706-1NX14-0AA0

Administration of up to 200 IP addresses

SNMP OPC Server Power Pack

V14

6GK1706-1NW14-0AC0

Extension from Basic to Extended

The SNMP OPC server software supports access to SNMP-capable devices in OPC client systems. Thus the diagnostics for individual devices is possible as well as diagnostics for the complete plant and device characteristics can be actively controlled. Scope and type of diagnostic information and control parameters depends on the respective scope of functions of the SNMP-capable devices.


2.4 Online Software Delivery

The following products of the SIMATIC NET DVD V14 can be delivered via Online Software Delivery:

Product

Version

MLFB

SOFTNET-IE S7 Lean (OSD)

V14

6GK1704-1LW14-0AK0

SOFTNET-IE S7 (OSD)

V14

6GK1704-1CW14-0AK0

HARDNET-IE S7 (OSD)

V14

6GK1716-1CB14-0AK0

HARDNET-IE S7 REDCONNECT (OSD)

V14

6GK1716-0HB14-0AK0

HARDNET-IE S7 REDCONNECT Power Pack (OSD)

V14

6GK1716-0HB14-0AK1

Note: Download delivery form (as of November 2016) is only available in the following countries (USA, Mexico, South Africa, Australia, India, Turkey, Brazil, Portugal, Spain, France, Switzerland, Italy, Luxembourg, Belgium, The Netherlands, Ireland, England, Austria, Germany, Norway, Sweden, Denmark, Finland, Poland, Czech Republic, Slovakia, Slovenia, Greece, Taiwan, South Korea, Argentina, Ecuador).

This delivery form has the advantage that software and licenses are available much faster and can be managed more easily.

The software products and licenses that can be downloaded have different order numbers.

They are ordered through the normal channels, e.g. the Industry Mall (http://www.siemens.com/industrymall).

Additional information about Online Software Delivery is available at the following link:
https://w3.siemens.com/mcms/topics/en/simatic/licenses/online-software-delivery/pages/Default.aspx


2.5 Trial Version SIMATIC NET DVD V14

Product

Version

MLFB

SIMATIC NET DVD V14

V14

6GK1700-0AA14-0AA0

2.6 Additional Details for PC Software DVD V14

Detailed information on the new SIMATIC NET PC software versions can be found in the files Liesmich / Readme which are also available on the SIMATIC NET DVD V14.

Liesmich.htm (619.3 KB)

Readme.htm (664.0 KB)

2.7 Upgrades and Software Update Service (SUS)

A specific Software Update Service is once again available for each of the SIMATIC NET PC products with V14; it expressly includes the delivery of upgrade packages.

Because this service does not depend on versions, the order numbers for the individual SUS packages have remained the same since 2007:

Software Update Service for

MLFB

SOFTNET-PB S7

6GK1704-5CW00-3AL0

SOFTNET-PB DP

6GK1704-5DW00-3AL0

SOFTNET-PB DP SLAVE

6GK1704-5SW00-3AL0

SOFTNET-IE S7

6GK1704-1CW00-3AL0

SOFTNET-IE S7 LEAN

6GK1704-1LW00-3AL0

SNMP OPC SERVER BASIC

6GK1706-1NW00-3AL0

SNMP OPC SERVER EXTENDED

6GK1706-1NX00-3AL0

HARDNET-PB S7

6GK1713-5CB00-3AL0

HARDNET-PB DP

6GK1713-5DB00-3AL0

HARDNET-IE S7 REDCONNECT

6GK1716-0HB00-3AL0

HARDNET-IE S7

6GK1716-1CB00-3AL0

SOFTNET-IE RNA

6GK1711-1EW00-3AL0


The following separate upgrade packages are also once again available for each SIMATIC NET PC product of V14:

Notes
You can find information about the selection of the required upgrade product here: 22090049

The correlation between the version numbers is explained here:


http://support.automation.siemens.com/WW/view/en/36456540


Software upgrade packages

MLFB

SOFTNET-PB S7
UPGRADE AS OF EDITION 2006

6GK1704-5CW00-3AE0

SOFTNET-PB DP
UPGRADE AS OF EDITION 2006

6GK1704-5DW00-3AE0

SOFTNET-PB DP SLAVE
UPGRADE AS OF EDITION 2006

6GK1704-5SW00-3AE0

SOFTNET-IE S7
UPGRADE AS OF EDITION 2006

6GK1704-1CW00-3AE0

SOFTNET-IE S7 LEAN
UPGRADE AS OF EDITION 2006

6GK1704-1LW00-3AE0

SOFTNET-IE S7 REDCONNECT VM
UPGRADE AS OF V8.2

6GK1704-0HB00-3AE0

SNMP OPC SERVER BASIC
UPGRADE AS OF EDITION 2006

6GK1706-1NW00-3AE0

SNMP OPC SERVER EXTENDED
UPGRADE AS OF EDITION 2006

6GK1706-1NX00-3AE0

HARDNET-PB S7
UPGRADE AS OF EDITION 2006

6GK1713-5CB00-3AE0

HARDNET-PBDP
UPGRADE AS OF EDITION 2006

6GK1713-5DB00-3AE0

HARDNET-PB CP56x3 DRIVER SOFTWARE
UPGRADE ON CD V7.1 and DVD V8.2

6GK1561-3AA01-3AE0

HARDNET-IE S7 REDCONNECT
UPGRADE AS OF EDITION 2006

6GK1716-0HB00-3AE0

HARDNET-IE S7
UPGRADE AS OF EDITION 2006

6GK1716-1CB00-3AE0

SOFTNET-IE RNA UPGRADE

6GK1711-1EW00-3AE0

Please bear in mind that you may initially experience longer than usual delivery times especially for the new SUS and Upgrade products.

3. Intended use

The standard user interface is the OPC interface to the OPC server. The OPC server itself is included in the scope of delivery of the respective software products. This means users have access via OPC as standard programming interface. The following OPC servers / OPC interfaces are included in the respective products:

3.1 PROFIBUS

Product

Includes OPC server/OPC interface for .....

HARDNET-PB DP

PROFIBUS DP
S5-compatible communication (FDL)

HARDNET-PB S7

S7 Communication

HARDNET-PB CP56x3 driver software

S5-compatible communication (FDL)
PROFIBUS DP (master), including DP Base
Access to DP slave of the CP 5614

SOFTNET-PB S7

S7 Communication

SOFTNET-PB DP

PROFIBUS DP
S5-compatible communication (FDL)

SOFTNET-PB DP slave

PROFIBUS DP (slave)

3.2 INDUSTRIAL ETHERNET / PROFINET / SNMP

Product

Includes OPC server/OPC interface for .....

HARDNET-IE S7
HARDNET-IE S7 REDCONNECT

S7 Communication
S5-compatible communication (SR)

SOFTNET-IE S7 Extended
SOFTNET-IE S7 / S7 Lean
SOFTNET-IE S7 REDCONNECT

S7 Communication
S5-compatible communication (SR)

SNMP OPC server

SNMP access via OPC

4. Additional information

The SIMATIC NET Manual Collection (10/2016) is included in the delivery of the SIMATIC NET DVD V14. In addition, it is included in the delivery of some additional SIMATIC NET products and therefore replaces the documentation / printed documentation of these products.

Contact for technical issues: Customer Support, Contact form



Avisos de Security
Para proteger a infra-estrutura técnica, sistemas, máquinas e redes contra ciberameaças é preciso implementar uma concepção holística de IT Security (e mantê-la continuamente) que corresponda ao padrão atual da tecnologia. Os produtos e soluções da Siemens formam somente um componente de uma tal concepção. Mais informações sobre Cyber Security você encontra em
https://www.siemens.com/cybersecurity#Ouraspiration.
Suporte para a estatística
Através desta função os IDs obtidos no resultado da busca serão exibidos conforme o número desejado (formato .txt)

Gerar lista
Copiar URL
Exibir esta página em novo design
Cockpit mySupport