×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109743758, Entry date: 04/24/2019
(0)
Rate

Firmware Update for ET 200pro EM 4 IO-Link HF

  • Entry
  • Associated product(s)
Firmware Update for ET 200pro EM 4 IO-Link HF

Description:

When firmware is updated, it must always be updated to the latest version available for the relevant article number. The previous versions of the firmware are only intended as a backup to enable you to downgrade to the original version.
The latest version of firmware in each case is valid for all revision levels of this article number.

A detailed description on performing the firmware update is provided in the entry109743764.

Overview of the article numbers and current firmware versions of the ET 200pro EM 4 IO-Link HF

Article number

Software
version

Upgrade by means of...

6ES7147-4JD00-0AB0

 V1.1.1

For Upgrade:
For a description, see below Update V1.1.1

For STEP 7 as of Version 5.5
 Registrierung notwendig  Classic_6ES7147-4JD00-0AB0_V111.ZIP (80,9 KB)
SHA-256 checksum (Information on SHA-256)
 Registrierung notwendig  Classic_6ES7147-4JD00-0AB0_V111.txt (1 KB) 


For STEP 7 TIA Portal
 Registrierung notwendig  TIA_6ES7147-4JD00-0AB0_V111.ZIP (81,0 KB)
SHA-256 checksum (Information on SHA-256)
 Registrierung notwendig  TIA_6ES7147-4JD00-0AB0_V111.txt (1 KB) 

 V1.1.0

Backup only:
For a description, see below Update V1.1.0

For STEP 7 as of Version 5.5
 Registrierung notwendig  Classic_6ES7147-4JD00-0AB0_V110.ZIP (80,2 KB) 

For STEP 7 TIA Portal
 Registrierung notwendig  TIA_6ES7147-4JD00-0AB0_V110.ZIP (80,2 KB)

V1.0.1

Backup only:
For a description, see below Update V1.0.1

For STEP 7 as of Version 5.5
Registrierung notwendig Classic_6ES7147-4JD00-0AB0_V101.ZIP (71.2 KB)

For STEP 7 TIA-Portal
Registrierung notwendig TIA_6ES7147-4JD00-0AB0_V101.ZIP (71.2 KB)

V1.0.0

Backup only:

For STEP 7 as of Version 5.5
Registrierung notwendig Classic_6ES7147-4JD00-0AB0_V100.ZIP (71.3 KB)

For STEP 7 TIA-Portal
Registrierung notwendig TIA_6ES7147-4JD00-0AB0_V100.ZIP (71.3 KB)


Update V1.1.1

The firmware V1.1.1 contains the following optimizations:

  • Improvement of the IO-Link communication during startup with COM3 devices
  • Improvement of the data backup of IO-Link devices with more than 69 parameters
  • Support for the FW update for IO-Link devices


Update V1.1.0

The firmware V1.1.0 comprises extensions for the I/O link configuration without S7-PCT.


Update V1.0.1

Firmware V1.0.1 contains the following optimizations:

  • Stability improvements during the download of the device parameters via S7-PCT.
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit