×
Siemens Industry Online Support
Siemens AG
Entry ID: 109743766, Entry date: 11/16/2018
(0)
Rate

Tools and Programs for Automation Technology (for STEP 7, WinCC, TIA Portal)

  • Entry
Overview of tools and programs for automation technology




SIEMENS provides selected tools and programs for different fields of automation. The topic-oriented organization helps you quickly find the tools and programs you required.  

Software - General


Compatibility Tool
The Compatibility Tool is a function provided by the Industry Online Support with which you can select compatible software products or check the compatibility of existing configurations.

Compatibility Tool for Automation and Drive Technology


TIA Selection Tool
The TIA Selection Tool provides you with wizards for selecting individual devices and complete systems.
It supports you in selecting modules and accessories, checks slotting rules and prevents selection errors.
You can use this tool to select and configure controllers, IO systems, HMI operator panels, Industry PCs, drive systems, switchgear, software, communication components, power supplies and industrial identification systems. You can also configure PROFIBUS and PROFINET networks including associated cables and connectors. 

TIA Selection Tool

 

SIMATIC Assessment Suite - Data Collector
The SIMATIC Assessment Suite - Data Collector (SAS-DC) - formally known as the SIMATIC Diagnostics Tool (SDT) - enables you to simply and easily collect diagnostics and system information from computers or other devices. 
How do you efficiently collect diagnostics and system information with the SIMATIC Assessment Suite - Data Collector (SAS-DC)?

 

Automation License Manager
SIMATIC Software is licensed with license keys. License keys can only be processed with the Automation License Manager (ALM) handling program that is on the associated CD and which is automatically installed by default with the software. 

Handling programs for authorizing or licensing SIMATIC products.


Controllers

Readiness Check Tool
You can use the TIA Portal Readiness Check Tool to simply check whether the hardware included in the project is supported by the TIA Portal.

TIA Portal Readiness Check Tool


Siemens Migration Studio: conversion of control software from Rockwell to Siemens

When migrating from a Rockwell system to a solution with SIMATIC S7-1500 you can either implement the control software right from scratch or convert it.

Siemens Conversion Studio: Migrating Controller Software from Rockwell to Siemens

 

Web Page Configurator for the ET 200SP AI Energy Meter ST
Using the free "Energy Meter Web Configurator" tool and matching block library you can configure web pages that are adapted to your plant configuration with the consumers connected via the Energy Meter. After downloading the HTML pages to the controller you can access the pages via the internet using a web browser and call up the consumption data of the connected nodes.
Web Page Configurator for the ET 200SP AI Energy Meter ST

 

New Primary Setup Tool (PST)
Using the Primary Setup Tool (PST) you can assign an address (IP address, for example) for SIMATIC NET network components, Ethernet CPs and gateways. 
New Primary Setup Tool (PST) version V4.2 HF1, 4.2 and 4.1 for setting addresses of SIMATIC NET Industrial Ethernet products available as download


SIMATIC Automation Tool
If you are managing a network with multiple devices, the SIMATIC Automation Tool can simplify processes and save time having a group of devices automatically processed with multiple processing threads. 

SIMATIC Automation Tool - the commissioning and service operation tool for SIMATIC modules

 
LOGO! Access Tool

Microsoft Excel add-in for reading and archiving data from LOGO! 8 in RUN.

LOGO! Access Tool

 

Safety Evaluation Tool
The Safety Evaluation Tool for the IEC 62061 and ISO 13849-1 standards takes you directly to your goal. This TÜV-tested online tool helps you to quickly and safely evaluate the safety functions of your machine. As a result you receive a standard-compliant report that can be integrated into the documentation as safety certification.

Safety Evaluation Tool

 

Operation and Monitoring


TIA Translation Tool
The TIA Translation Tool is used for convenient management and translation of multilingual project texts of a Totally Integrated Automation Portal project.

TIA Translation Tool
TIA Translation Tool Configuration Instructions

 

Export Graphics Tool
The "Export Graphics Tool" exports all graphics from your WinCC (TIA Portal) configuration into a directory of your choice. The original file type and object properties (transparency, for example) are retained in this case. This permits you to process graphics with the usual graphics programs and then integrate them back into the project.
Export Graphics Tool: Exporting graphics from WinCC (TIA Portal) to a local directory

 

SIMATIC HMI Label Creator
Many of the SIMATIC HMI operator panels give you the option of custom labeling and configuring the control buttons. Using the SIMATIC HMI Label Creator you can quickly and easily create labeling strips.
SIMATIC HMI Label Creator: individual labels for HMI devices and Panel PC systems

 

Sm@rtServiceMonitor
The Sm@rtServiceMonitor reads out the current Sm@rtClient connections and forwards them to the HMI Runtime for further processing. With this tool you can monitor remote access and stop operators locally as required.
Available as application example:

Remote Access to SIMATIC HMI Operator Panels


PH-HWAdvisor
tThis tool helps you determine suitable hardware for the Process Historian 2014.

Determination of suitable hardware for the Process Historian 2014 with the "PH-HWAdvisor" tool

 

Web Page Configurator for the ET 200SP AI Energy Meter ST
Using the free "Energy Meter Web Configurator" tool and matching block library you can configure web pages that are adapted to your plant configuration with the consumers connected via the Energy Meter. After downloading the HTML pages to the controller you can access the pages via the internet using a web browser and call up the consumption data of the connected nodes.

Web Page Configurator for the ET 200SP AI Energy Meter ST


Toolbox for HMI projects
The HMI Toolbox provides a variety of useful tools to help you with your daily work. 
The HMI Toolbox includes tools for six different topics. There is separate documentation and a global library or ZIP archive for each topic.

Toolbox for HMI Projects


SIMATIC HMI Option+
SIMATIC HMI Option+ provides completely new functions for your SIMATIC HMI Comfort Panel. In addition to configuration of the device interfaces from Runtime, this application also offers you options for user identification by RFID card.

SIMATIC HMI Option+

 


IPC and PC-based



SIMATIC IPC DiagBase
Using the SIMATIC IPC DiagBase diagnostics software allows you to recognize early on any potential faults on SIMATIC IPCs and helps you to prevent or reduce system downtimes.
SIMATIC IPC DiagBase - Download

 

IP Config Tool for SIMATIC IPCs with WinAC RTX
This tool supports you when configuring the network adapters of SIMATIC IPCs with WinAC RTX installed.
IP Config Tool for SIMATIC IPCs with WinAC RTX

 

SITOP UPS Manager for SITOP UPS1600
You use the SITOP UPS Manager to configure the SITOPUPS1600 uninterruptible power supply via a USB or Industrial Ethernet connection.
SITOP UPS Manager for SITOP UPS1600


Networks and Communication


PRONETA Commissioning and Diagnostics Tool for PROFINET
PRONETA is a free tool for the analysis and configuration of PROFINET networks with special support for ET 200 distributed IO. The IO Test provides support for the quick and convenient examination and documentation of a plant's wiring.

PRONETA Basic 3.0.0.1 Commissioning and Diagnostics Tool for PROFINET

 

Overview of performance data
Right in the planning phase of a plant it is important to estimate the reaction times in a system consisting of controllers, remote IOs, PCs and also components of industrial identification. With the measured performance data for industrial communication with SIMATIC S7 components you receive reliable information.

Performance data overview

 

Security Configuration Tool (SCT)
The Security Configuration Tool (SCT) configuration software helps you to configure the security functions of specific SCALANCE products, CPs and SOFTNET Security Clients.
Download of the Security Configuration Tool (SCT) V4.2 configuration tool
Latest information on the Security Configuration Tool (SCT)
SIMATIC NET: License Conditions for Security Configuration Tool (SCT)


 

Drive Technology


SIZER for Siemens Drives
The SIZER for Siemens Drives configuration tool decisively simplifies the engineering of low-voltage drive systems. Starting from your application, the tool supports you step-by-step when defining the mechanical system as well as when selecting and dimensioning converters, motors and gear units.

SIZER for Siemens Drives

 

SINAMICS XML Parser
For SINAMICS drives there are XML files available with the possible warning and error codes of each drive. These XML files that are supplied with the drive’s firmware also include these messages in plain text.
To allow easy and effective use of this information from the XML files, for example, for visualization, this XML data must be converted to a suitable file format.

Transforming warning and error messages of a SINAMICS drive with the aid of the XML parser and integrating them into a STEP 7 / HMI project



General Topics


Compatibility Tool for Automation and Drive Technology
TIA Selection Tool
   



Further Topic Pages

 

Major Topics at a Glance
SIMATIC HMI in the Online Support
TIA Portal - An Overview of the Most Important Documents and Links - Visualization
Migration of Plants with SIMATIC (TIA Portal) - Visualization
Machine-oriented operator control and monitoring in the Online Support
SIMATIC HMI Devices
SIMATIC Apps: An Overview of the Most Important Documents and Links
SIMATIC WinCC in the Online Support
SITOP Power Supply Systems in the Online Support
Energy Data Acquisition in the Online Support
Energy Management with SIMATIC in the Industry Online Support
Energy Data Management with the SIMATIC Energy Manager PRO in the Online Support
SIMATIC Energy Suite in the Online Support
SIMATIC powerrate in the Online Support