×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109744163, Entry date: 07/02/2019
(6)
Rate

How do you load the project data if the version of the firmware installed in the S7-1500 CPU cannot be selected in the hardware catalog of your version of STEP 7 (TIA Portal)?

  • Entry
  • Associated product(s)
You can also load the project data into the S7-1500 CPU even if there are differences between the configured module and the destination module (online).

Description
A specific version of STEP 7 (TIA Portal) is required to configure a firmware version in the device configuration. For example, to configure the firmware version V2.6 for the S7-1500 CPU you need STEP 7 Professional V15.1 (or higher). The following table gives you an overview of the version of STEP 7 Professional you need to be able to configure the desired firmware version.
 

Firmware of the S7-1500 CPUVersion of STEP 7 Professional (or higher)
V2.6V15.1
V2.5V15
V2.1V14 SP1
V2.0V14

You can also load the project data into a S7-1500 CPU if the firmware version of that CPU is not available in the hardware catalog of STEP 7 (TIA Portal).

Example
In STEP 7 (TIA Portal) V15, in the device configuration you cannot select the S7-1500 CPUwith firmware V2.6 (or higher). There will not be an HSP for the S7-1500 with firmware V2.6 for STEP 7 (TIA Portal) V15.
However, the project data that you created in STEP 7 (TIA Portal) V15 for an S7-1500 CPU with firmware V2.5 you can load into the S7-1500 CPU with firmware V2.6. For this you must select the firmware V2.5 in the device configuration for your CPU.
When downloading the project data into the CPU a warning indicates the differences between the CPU (with firmware V2.5) in the device configuration and the CPU (with firmware V2.6) actually installed in the rack. Ignore this warning.

Note
However, if you want to use the new functions of the S7-1500 CPU added since firmware version V2.6, you have to use STEP 7 (TIA Portal) V15.1 and configure a CPU with firmware V2.6.

Further Information
More information is available at the links in the following table:
 

Entry typeLink 
FAQWhy does the delivered module have a different article number to the one ordered? 
FAQHow do you convert STEP 7 Professional / Basic projects in TIA Portal V14, which you have created in earlier versions of TIA Portal? 
DownloadFirmware Update for S7-1500 CPUs incl. Displays and ET 200 CPUs (ET 200SP, ET 200pro) 

 


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.