×
Siemens Industry Online Support
Siemens AG
Тип сообщения: Часто задаваемые вопросы ID сообщения: 109744163, Дата сообщения: 03.04.2020
(21)
Оценить

How do you load the project data if the version of the firmware installed in the S7-1500 CPU cannot be selected in the hardware catalog of your version of STEP 7 (TIA Portal)?

  • Сообщение
  • Относится к продукту(ам)
You can also load the project data into the S7-1500 CPU even if there are differences between the configured module and the destination module (online).

Description
A specific version of STEP 7 (TIA Portal) is required to configure a firmware version in the device configuration. For example, to configure the firmware version V2.8 for the S7-1500 CPU you need STEP 7 Professional V16 (or higher). The following table gives you an overview of the version of STEP 7 Professional you need to be able to configure the desired firmware version.
 

Firmware of the S7-1500 CPUVersion of STEP 7 Professional (or higher)
V2.8V16
V2.6V15.1
V2.5V15
V2.1V14 SP1
V2.0V14

You can also load the project data into a S7-1500 CPU if the firmware version of that CPU is not available in the hardware catalog of STEP 7 (TIA Portal).

Note
The projected firmware version and the firmware on the CPU do not have to be identical. Configurations with earlier versions of STEP 7 (TIA Portal) that did not yet have a certain firmware status in the catalog can be used in an upward compatible manner.

Example
You had configured the firmware V2.6.1 in the device configuration for the S7-1500 CPU. However, the last firmware update of your CPU is V2.8.1. But you can commission the CPU with firmware version V2.8.1 with the configured firmware version V2.6.1.

  • When downloading the project data into the CPU a warning indicates the differences between the CPU (with firmware V2.6.1) configured in the device configuration and the CPU actually in the rack (with firmware V2.8.1). Ignore this warning.
  • The corrections and improvements of firmware V2.8.1 are implemented and do not require a new configuration with firmware version V2.6.1.
  • However, if you want to use the new functions of the S7-1500 CPU added since firmware version V2.8.1 you have to use STEP 7 (TIA Portal) V16 and configure a CPU with firmware V2.8.1.

Further Information
More information is available via the links in the following table:
 

Entry typeLink 
FAQWhy does the delivered module have a different article number to the one ordered? 
FAQHow do you convert STEP 7 Professional / Basic projects in TIA Portal V14, which you have created in earlier versions of TIA Portal? 
DownloadFirmware Update for S7-1500 CPUs incl. Displays and ET 200 CPUs (ET 200SP, ET 200pro) 

 


Указания по безопасности
Для обеспечения и дальнейшего поддержания кибер-безопасности технической инфраструктуры, систем, машин и сетей необходимо внедрить комплексную концепцию информационной безопасности, которая соответствует последним достижениям науки и техники. Продукты и решения Сименс являются всего лишь одним из компонентов такой концепции. Более подробную информацию о кибер-безопасности можно получить здесь
https://www.siemens.com/cybersecurity#Ouraspiration.
Оценить сообщение
без оценки
Вопросы и обратная связь
Что вы хотите сделать?
Примечание: отзыв всегда относится к текущей статье. Ваше сообщение будет отправлено редакторам службы онлайн-поддержки. В течение нескольких дней вы получите ответ, если ваш отзыв содержит вопрос. Если у нас не возникнут вопросы по вашему отзыву, мы не будем вас беспокоить.
Поддержка статистики
Данная функция позволяет выдавать идентификаторы (ID) результата поиска согласно желаемому количеству (формат .txt)

Генерировать список
Копировать URL
Отобразить эту страницу в новом дизайне
Панель управления mySupport
Тематические страницы для данных записей