×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109744337, Entry date: 02/24/2017
(7)
Rate

How to you connect the communication module CM 1542-5 or the communications processor CP 1542-5 as I slave in STEP 7 V5.x to an S7-300/S7-400 CPU?

  • Entry
  • Associated product(s)
With the communication module CM 1542-5 and the communications processor CP 1542-5 you can operate an S7-1500 as I slave on a PROFIBUS DP master system.

The following instructions show you how to connect the CM 1542-5 as I slave in STEP 7 V5.x to an S7-300/S7-400 CPU.

  109744337_CM1542-5_ISlave_en.pdf (625,9 KB)

Note
You use the same procedure as for the CM 1542-5 to connect the CP 1542-5 as I slave in STEP 7 V5.x to an S7-300/S7-400 CPU.


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.