×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109744655, Entry date: 04/01/2021
(0)
Rate

IP65 stainless steel keyboard and keyboard tray for 16:9 PRO devices

  • Entry
  • Associated product(s)
This product is sold out.

For successor see SIOS entry ID:  109760419 


___________________________________________________________________________________________________

Product note from 2017: 

The existing IP65 stainless steel keyboard and keyboard tray for the 4:3 PRO devices in dark gray are being adapted in color for the new 16:9 PRO devices: Both products will be available in silver, matching the new PRO devices. These products belong to the system components for PRO devices which are only suitable for SIMATIC HMI/IPC PRO devices.


Customers can use the keyboard or the keyboard tray during commissioning or normal operation for data input or tool storage. These products can be mounted to the underside of the PRO devices.

The stainless keyboard has all-round IP65 protection and offers utmost operating convenience and a comfortable tactility. The keyboard is connected via a USB port. The mouse (left and right mouse buttons) is controlled with integrated keys. The four arrow keys are used for navigation. The function corresponds to that of a standard keyboard. The mouse pointer cannot be moved directly. A separate mouse or mouse pad is required to this purpose. With the help of the tilting adapter, you can adjust the keyboard to the best operating position.



Color example. Original color matching the PRO basic device (color: silver)
 


The keyboard tray made of powder-coated aluminum has two externally accessible USB ports that can be used to connect a keyboard, a mouse or for quick data backup on a USB stick. A closed protective cover provides all-round IP65 degree of protection for all USB ports. The tray can be adjusted vertically with the help of the tilting adapter.




Color example. Original color matching the PRO basic device (color: silver)
 



Design:

The stainless steel keyboard and the keyboard tray are mounted below the PRO device:  



 



The figure shows an example of the installation of the IP65 stainless steel keyboard to the PRO device using the basic adapter. The keyboard tray is installed in the same way.

Note: 

For the SIMATIC PRO device of the type "prepared for support arm and extension components  (round pipe connection)", a basic adapter must also be purchased for installing a keyboard/keyboard tray (Article number: 6AV7674-1KA00-0AA0).






Additional technical and graphic data on the stainless steel keyboard and keyboard tray can be found in the "Product Support" of the Industry Online Support: https://support.industry.siemens.com/cs/ww/en/view/109745038  


The following table shows the complete order overview:

 Article number 

 Content

6AV7674-1NE00-0AA0

IP65 stainless steel keyboard for PRO devices with 16:9 display

6AV7674-1NE01-0AA0

Tool and keyboard tray for PRO devices with 16:9 display

 

The 3D Step files can be downloaded here:

 Registrierung notwendig  6AV7674-0NE00-0AA0_Keyb_PRO.zip (1.4 MB)

 Registrierung notwendig  6AV7674-1NE00-0AA0_Keyb_PRO.zip (1.4 MB)

 Registrierung notwendig  6AV7674-0NE01-0AA0_Ablage.zip (556.8 KB)

 Registrierung notwendig  6AV7674-1NE01-0AA0_Ablage.zip (556.8 KB)









Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.