×
Siemens Industry Online Support
Siemens AG
Entry type: Download, Entry ID: 109744950, Entry date: 04/10/2017
(30)
Rate

USB Recovery (Reset to factory) Mode for 2nd Generation Basic Panels

  • Entry
  • Associated product(s)
This software enables you to do a reset to factory settings for your Basic Panel 2nd Generation.

This software has been released for the following devices:

  • KTP400 Basic
  • KTP700 Basic / KTP700 Basic DP
  • KTP900 Basic
  • KTP1200 Basic / KTP1200 Basic DP


How to do a reset to factory settings for your Basic Panel 2nd Generation


Requirements

  • The USB stick have to be provided in FAT32 format.
  • The USB stick have to be provided with USB version 2.0 or lower.
  • The HMI device image file must be provided with Version V14.

Procedure

  • Unpack the file "Basic2nd_Recovery_System.zip" directly on the USB Stick into the main directory.
  • Copy the suitable HMI device image file into the path "SIMATIC.HMI\Recovery\" on the USB stick (file type "*.fwf").

Note: You can find the HMI device image file under
"Programs\Siemens\Automation\Portal V14\Data\Hmi\Transfer\14.0\Images".

  • Shut down the HMI device.
  • Plug the USB stick into the USB interface of the HMI device
  • Switch on the HMI device.
  • To reset the HMI device to the factory settings, press the button "START RECOVERY (..3..)" three times and follow the instructions shown on the display. At the end of the recovery process, remove the USB stick and press the "REBOOT" button.

Download

Name

link

SHA-256 checksum

Date

Basic2nd Recovery Stick

 Download unterliegt Exportcontrolle  Basic2nd_Recovery_System.zip (24,6 MB)


7c0af5ff9529848994a58cd5d0be7648

1b5a89eb23b2f06f241d6ff5e97f6aa3

03/2017

Open Source software components

Registrierung notwendig RescueStick_Readme_OpenSrcSW.zip (559.6 MB)

c90673d53cfa669454a0856dbea51dfd

22f93010caf301b2acc204bf9bddd9e0


03/2017

Note:
How you can determine the SHA-256 checksum of a file is described in the article with the entry ID 109483101


Search Item : USB Rescue Stick , USB Recovery Mode 

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.