×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109744966, Entry date: 02/13/2017
(1)
Rate

SIMATIC Logon V1.5 SP3 Update 2

  • Entry
  • Associated product(s)
Update 2 is available for SIMATIC Logon V1.5 SP3.

What is new?
SIMATIC Logon V1.5 SP3 Update 2 fixes a security vulnerability. For more information, see Security Advisory http://www.siemens.com/cert/pool/cert/siemens_security_advisory_ssa-931064.pdf.
    
Readme
Read the information in the following Readme file
  
 Registrierung notwendig SIMATIC_LOGON_01_05_03_02_Readme.zip (371,6 KB) 
  
Installation file
The following ZIP file contains the installation file required for the update.
 
  Registrierung notwendig SIMATIC_LOGON_01_05_03_02.zip (235,9 MB) 
 
Note
In order to keep your system continuously up-to-date, please note the information in the compatibility tool: www.siemens.de/kompatool 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.