Entry type: Product note, Entry ID: 109745365, Entry date: 02/17/2017
(0)
Rate

Delivery release for the manual transfer switching equipment 3KC (MTSE)

  • Entry
  • Associated product(s)
New manually operated transfer switching equipment (MTSE) is now available in addition to the automatic (ATSE) and remotely operated (RTSE) 3KC transfer switching equipment. The 3KC transfer switching equipment offers reliable switchover between two current sources. It ensures a reliable power supply in the event of line fluctuations.



3KC

The new manually operated transfer switching equipment (MTSE) 3KC0 with 16 A to 1600 rated uninterrupted current offers reliable switchover between the main network and an alternative network in order to ensure a consistent power supply. The manually operated transfer switching equipment can also be used as a load transfer switch for switchover between two loads. The 3KC transfer switching equipment consists of two switch connectors which are joined by a mechanical interlock. It is approved according to IEC 60947-6-1 and IEC 60947-3.

In addition to the 3KC0 transfer switching equipment, the 3KC portfolio includes the following accessories:

- Direct operating mechnism
- Door-coupling rotary operating mechanisms
- Phase barriers
- Terminal covers
- Bridging bars
- Additional poles
- Auxiliary switches


Target market:
Worldwide application China: CCC about 6 months after start of delivery


Start of delivery:

ProductSupport.EntityResultListTitle
ProductSupport.EntityResultListDescription

ProductSupport.EntityResultListButtonText
Copy URL
mySupport Cockpit