×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109745386, Entry date: 07/27/2017
(7)
Rate

SIMATIC S7-1500: Rapid Traverse/Creep Speed Positioning (2SpeedPositioning)

  • Entry
  • Associated product(s)
Rapid traverse/creep speed positioning moves an axis to a specified target position in a relatively simple way. The traversing motion is performed with the aid of two speed levels and suitable switchover points.

An axis can be positioned in many different ways. In this context, especially TIA Portal with the S7-1200 and S7-1500 controller families provides support in the form of technology objects. Very high positioning accuracy of the axis can be achieved. However, this is also reflected in the hardware used to control these axes.
If an axis is to be positioned with relatively little hardware or with lower, controlled accuracy, this can be achieved with the aid of position monitoring and a simple contactor circuit. To this end, the positioning axis can be moved at two different speeds and simply switched off at the desired target position at the appropriate time using a contactor. With this method, called rapid traverse/creep speed positioning, relatively high positioning accuracy of the axis can be achieved.

Controlled positioning in rapid traverse/creep speed mode first moves the positioning axis towards the target position at a high speed (rapid traverse). At a defined position, the speed is switched to a lower speed (creep speed) at which the axis can then be moved to the target position.



To implement the two speed levels of rapid traverse/creep speed positioning, for example, pole-changing motors with a simple contactor circuit or simple frequency converters that allow speed selection through digital inputs can be used. The axis position can be detected with incremental or absolute encoders.

Documentation and Sample Project
  Documentation (2,4 MB)
 Registrierung notwendig  Library for TIA Portal V14 (980,8 KB)
 Registrierung notwendig  Library for TIA Portal V15 (1,2 MB)
 Registrierung notwendig  Sample project for TIA Portal V14 (1,2 MB)
 Registrierung notwendig  Sample project for TIA Portal V15 (2,3 MB)


Last Changes
Code correction of actual value calculation


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.