×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109745493, Entry date: 04/04/2017
(0)
Rate

Siemens Network Planner – Device Descriptions Update 01

  • Entry
  • Associated product(s)
Attached please find the topical device descriptions for Siemens devices for SINETPLAN V1.0 for downloading.


Description

The update includes additional Siemens devices, which are not included in the catalog with SINETPLAN V1.0.

Further, some of the existing device descriptions will be replaced by updated device descriptions.

Following the installation, the catalog of SINETPLAN will include the new respectively updated devices for planning.

The procedure to be applied to update the device catalog of a SINETPLAN installation with this download is described in the SINETPLAN_SD_update_readme.pdf as well as the supplements to SINETPLAN V1.0 under the following entry ID: 109738284




Content of the device descriptions, Update 01:


  • AS products, e.g. S7-1500 CPU
  • CI products, e.g. Switches X200 Family
  • MC products, e.g. Sinamics
  • Legacy, update of existing descriptions




Downloading the update:


Registrierung notwendig SINETPLAN_SD_Update_01_AS_Products.zip (1.0 MB)

Registrierung notwendig SINETPLAN_SD_Update_01_PD_PA_CI_Products.zip (1.9 MB)

Registrierung notwendig SINETPLAN_SD_Update_01_MC_Products.zip (187.6 KB)

Registrierung notwendig SINETPLAN_SD_Update_01_Legacy.zip (24.0 KB)


Registrierung notwendig SINETPLAN_SD_update_readme.pdf (253.1 KB)





Checksums:


AS products:

CI products:



MC products:



Legacy:





Notes about downloading
The software is subjected to export restrictions. Download is only possible for registered users. Please note that, on account of the strong demand, the registration for export-restricted downloads will take some time.


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit