×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109745561, Entry date: 08/14/2019
(5)
Rate

MindConnect Nano – Firmware and Open Source Software (OSS)

  • Entry
  • Associated product(s)
This firmware version is valid for all MindSphere regions (EU1, EU2 and CN1)

Note:

  • For MindSphere on Alibaba Cloud in region China 1 Version V3.3.0.4 is the minimum required version.
  • Not all features are available in each region at the same time. Please refer to the release notes.


MindConnect – MindSphere V3 Firmware (Update August 2019)

First of all the MindConnect has to be set to factory settings. (Only necessary if the Box was already connected to V2 MindSphere)

1. Create a “ConBox_Commands.json” file (e.g. with Notepad)

JSON format

{

  "Commands": [

   {

    "Cmd": "DoFactoryReset",

    "DeviceID": "_MindConnect_ID_"

   }

  ]

}

The label “_MindConnect_ID_” has to be replaced with the ID which is located on the label of the MindConnect Box. The number is right below the article number.


2. 
Put it on a USB stick and plug the stick in the MindConnect

3. The MindConnect will be restarted automatically

The network and SAL settings will be reset to their initial state on MindConnect. All SAL and script logging files will be then deleted.

To load new firmware on your MindConnect hardware please follow these steps:

1. Download the firmware ZIP file.

Version August 2019:  Registrierung notwendig  03.03.00.05_b021_NANO.zip (94,9 MB) 

SHA256: 592EA2EC6E2BEE66B304DBA467C404DFB20CD1E5230C4B9393024A9E29DBB421

2. Extract the firmware.

3. Copy the extracted/unzipped fw.tar file to a USB stick (fat32 formatted).

4. Insert the USB stick and wait until the firmware update is complete.

  • Update carried out: ERROR LED flashes orange
  • MindConnect hardware reboots
  • MAINT LED flashes orange for a few seconds
  • RUN LED orange (not connected to MindSphere)

5. Disconnect the USB stick.

6. Ready.

Note: During the firmware update of the device the data collection will be stopped for a short time frame. So some data points will be lost. 

More Information: Getting connected to MindSphere V3 109755908

Open Source Software (OSS)

Version November 2018:  Registrierung notwendig  ReadMeOSS_Nano.zip (669,0 MB) 

SHA256: EC3C58BAC963832C38B177161E1EEFB893F17FA9FAFC045ED604010FF8EEC08B


Firmware Update Guide

Current versionUpdate to
< V01.00.01.02 b002= V01.00.01.02 b002
< V01.02.04.00 b002= V01.02.04.00 b002
= V01.02.04.00 b002Current V3 version (see above)


V01.00.01.02 b002:

Version September 2016:  Registrierung notwendig  Nano_01.00.01.02_b002.zip (44,9 MB)
SHA256: 324431BFE9482F13B7843176ADF7461BE0B64082A50E1F0B848D7DD95376E602

V01.02.04.00 b002:

Version July 2018:  Registrierung notwendig  Nano_01.02.04.00_b002.zip (36,6 MB)
SHA256: DA8CF71604D0DAF9824E73DB06147FFBEAAA54781C162699A70FF4E61C51E835

Open Source Software (OSS)

Version August 2017:  Registrierung notwendig  MindConnect_NANO_1.3_OSS.zip (314,8 MB) 
SHA256: 6D93E5E380AFE160F54C96DFDCE5567A5735C3DE6128045F5D2B43FD922B0E5D

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.