×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109745764, Entry date: 04/30/2019
(4)
Rate

S7-1500T: Synchronizing in Standstill "LCISS_CamInStandStill" / "LCISSM_CamInStandStillMultiple"

  • Entry
  • Associated product(s)
This application example shows how to couple the leading axis and one or more following axes via setpoint positions in standstill with camming using the instruction "MC_CamIn".

Synchronizing in Standstill with one following axis "LCISS_CamInStandStill"
To couple the leading axis and the following axis, these axes have to be in the synchronous position. You can use the "CamInStandStill" function block to move the following axis or the leading axis to the synchronous position and to synchronize them afterwards.

This application example describes how to synchronize a following axis (slave) to a leading axis (master) with a S7-1500T.

In the "LCISS_CamInStandStill" function block, the following synchronizing modes are realized:

  • If the leading axis is already in the synchronous position, the following axis will be moved to the synchronous position and will be synchronized.
  • If the following axis is already in the synchronous position, the leading axis will be moved to the synchronous position and will be synchronized.

The desired synchronizing mode can be selected via the "syncMasterToSlave" parameter.

The individual steps of the coupling via dynamics parameters are programmed in the "LCISS_CamInStandStill" function block (FB). 




Documentation and example projects



Synchronizing in Standstill with more following axes "LCISSM_CamInStandStillMultiple"

This application example describes how to synchronize a following axes (slaves) to a leading axis (master) with a S7-1500T.
The individual steps of the coupling via dynamics parameters are programmed in the "LCISS_CamInStandStill" function block (FB). 




Documentation and example projects
  Documentation (964,5 KB)
 Registrierung notwendig  Project and Library for STEP 7 V14 SP1 (1,8 MB)
 Registrierung notwendig  Project and Library for STEP 7 V15.1 (2,4 MB)


Further Information
Application example – Circular Motion on the Basis of Cam Disks “MoveCircle2D”

Last Changes
Project for TIA Portal V15.1
Query "CommandAborted for MoveMaster and MoveSlave added


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit