×
Siemens Industry Online Support
Siemens AG
Entry type: Product note, Entry ID: 109745984, Entry date: 03/31/2017
(13)
Rate

Delivery Release for STEP 7 V14 SP1

  • Entry
  • Associated product(s)
Service pack 1 for STEP 7 V14 available


SIMATIC STEP 7 Professional / Basic V14 SP1

The Service pack 1 for SIMATIC STEP 7 Professional V14 and STEP 7 Basic V14 is available for delivery. This will be supplied within the scope of the corresponding Software Update Service contracts.

You can find what's new for other TIA Portal products on the following page: 109744304 

Important information:

When installing the various TIA Portal products and options, ensure that you use the same versions of service packs for the installation. For example, if you have installed SP1 for STEP 7 V14, you must also install SP1 for WinCC V14. Service packs must be installed at the same time for all products. Do not start the TIA Portal until you have upgraded all products.

Please note that not all TIA Portal V14 SP1 products are available concurrently.


Highlights SIMATIC STEP 7 V14 SP1

STEP 7 V14 SP1 includes new features for all phases of the engineering workflow. An overview of the new functions is available here:

Hardware configuration

  • New power supply PS 60W 24/48/60VDC HF for S7-1500 with energy buffering for up to 20 MB of data backup in the CPU
  • Tabular configuration of the IO channels for modules ET 200MP DI HF and HF ET 200MP DO including copy and paste, and auto fill function
  • Editing device names in the graphical views
  • Improved zoom behavior and optimized (multi-) selection in the graphical network and topology views
  • Overview of IO tags of an entire device (such as an ET 200SP station)
  • Easy removal of unused GSD files in the project
  • Wizard extension for UDP Multicast in the Open User Communication (OUC) with S7-1500

Editors for programming languages
  • Structured tags and ARRAY elements can be replaced by other tags using drag-and-drop in the SCL program code.

  • You can toggle between insert and overwrite mode in the SCL editor.

  • In SCL, selected program code segments can be easily enclosed with certain structural elements, such as "If...then".

  • A detailed comparison of individual blocks can be started directly from the project tree (offline/offline, but also online/offline).

  • The tag comment can be displayed directly at the point of use in LAD/FBD.

  • The F7 function ("Open block/PLC data type...") can also be started with focus within editors.

  • Generating an external source file from blocks: The export of objects as an external source includes PLC data types (UDT) defined in the block interface, multiple instances and all blocks called.

  • In the "Instructions" task card, all controller instructions used are updated to the latest version.

New instructions

  • The new "SCATTER" and "GATHER" instructions for S7-1200 (firmware V4.2 or higher) and S7-1500 (firmware V2.1 or higher), enables values to be copied between tags of the BYTE, WORD, DWORD, LWORD data types and tag ARRAYs of the BOOL data type. For example, this enables control and status words of individual plant units to be separated into the individual bit signals and easily reassembled.

  • Using the "GetSMCInfo" instruction for S7-1500 (firmware V2.1 or higher), you can read information in the user program about the inserted SIMATIC Memory Card, for example, the memory capacity, the allocated space or the number of write/delete operations already performed (percentage).

  • The "Polyline" instruction for S7-1200 (firmware V4.2 or higher) and S7-1500 (firmware V2.0 or higher) maps the input value of a characteristic curve to the initial value. The characteristic curve is defined as a polygon (with up to 50 interpolation points).

Language innovations

  • PLC data types (UDT) and ARRAY comments can be changed for specific instances.

  • It is possible to assign different PLC data types (UDTs) with the same structure but different symbolic names.

  • S7-GRAPH blocks as of version 4.0 enable initial value acquisition of the faulty operands. The actual values of the signal states of Boolean operands and the results of comparators in interlocks and transitions are continuously recorded from the time the initial value acquisition was activated, even if no error occurs. The signal states are stored in the GRAPH instance data block every cycle. A maximum of 32 signal states are recorded per interlock or transition of a GRAPH step.

Libraries

  • Project libraries and global libraries can now be translated separately into other foreign languages.

  • Simplified upgrading of types (blocks, PLC data types) in an existing project library.

  • The user-defined help can now also be launched in the context of the project language. Prior to V14, this was only possible in the context of the TIA Portal language.

Messages / Diagnostics

  • The presentation of the alarm display in the inspector window has been improved and functionally enhanced with new features such as "Receive alarms" and "Freeze alarms".

Migration

  • The local constants used in SCL sources for ARRAY limits are retained when migrating STEP 7 V5.x to the TIA Portal.

Trace

  • Switching display formats (for example: A WORD can be represented as hexadecimal, signed or unsigned INT)

  • The scrollbar the X-axis has a small preview window ("Time range display"), in which you can identify the area you just zoomed.

System functions

  • CAx data based on XML for communicating with ECAD systems, for example, can be exported and re-imported.

  • Users can freely define cross-references, for example, to determine multiple accesses of tags.

  • The TIA Portal can be connected to external password management via a password provider. The advantage of this is that passwords need not be disclosed. This increases the security of the program code.

SIMATIC Ident

The technology object (TO) for SIMATIC Ident combines the hardware configuration of communication modules and readers with programming an S7-1200 and S7-1500 controller. The TO prevents incorrect settings and detects errors in the configuration.

Hardware configuration:

  • Each communication module / reader is given a "unique name" by system manufacturers with which it is identifiable by commissioning engineers and programmers alike.

  • The configuration of each communication module, reader or reading point is set via the TO.

  • You can use the "Auto-configuration" button to configure identification devices for the operation with the TO with a single click.

You can find a document with an overview of the new functions in delivery release of TIA Portal V14 SP1: 109744304 


SIMATIC STEP 7 V14 Product Information

System requirements

STEP 7 Professional / Basic V14 SP1 are released for use with the following operating systems (64-bit only):

Windows 7 (64-bit)

  • Windows 7 Home Premium SP1 (STEP 7 Basic only)

  • Windows 7 Professional SP1

  • Windows 7 Enterprise SP1

  • Windows 7 Ultimate SP1

Windows 8.1 (64-bit)

  • Windows 8.1 (STEP 7 Basic only)

  • Windows 8.1 Professional

  • Windows 8.1 Enterprise

Windows 10 (64-bit, new with V14 SP1)

  • Windows 10 Home Version 1607 (STEP 7 Basic only)

  • Windows 10 Professional Version 1607

  • Windows 10 Enterprise Version 1607

  • Windows 10 Enterprise 2016 LTSB

  • Windows 10 Enterprise 2015 LTSB

Windows Server (64-bit)

  • Windows Server 2008 R2 StdE SP1 (STEP 7 Professional only)

  • Windows Server 2012 R2 StdE

  • Windows Server 2016 Standard


The following table shows the recommended hardware for operating STEP 7.

HardwareRecommendation
ComputerSIMATIC Field PG M5 Advanced or higher (or comparable PC)
ProcessorIntel® Core™ i5-6440EQ (2.7 GHz)
RAM16 GB or more (for large projects 32 GB)
Hard diskSSD with at least 50 GB free storage capacity
Network1 Gigabit (for multi-user)
Monitor15.6" full HD display (1920 x 1080 or larger)


Compatibility with other products

STEP 7 Professional / Basic V14 SP1 works together with WinCC, Startdrive, SIMOCODE ES and SOFT STARTER ESV14 SP1 and SIMOTION SCOUT TIA V5.1 in a single framework.

STEP 7 Professional / Basic V14 SP1 (incl. WinCC Basic V14 SP1) can be installed on a PC in parallel with other versions of STEP 7 V11 to V13 SP2, STEP 7 V5.5 SP4 (STEP 7 V5.6), STEP 7 Micro/WIN V4.0 SP9, WinCC flexible 2008 SP3 and WinCC (from V7.3).

A project upgrade to TIA Portal V14 is performed exclusively on the basis of TIA Portal V13 SP1 projects (last update recommended). In order to provide you with the best possible support, the latest version of V13 SP2 is included with the V14 SP1 products. A compatibility mode is not supported.

Supported virtualization platforms

  • VMware vSphere Hypervisor (ESXi) 6.0
  • VMware Workstation 12.5
  • VMware Player 12.5
  • Microsoft Hyper-V Server 2016

Supported operating systems for virtualization platforms as host operating system

  • Windows 7 Professional/Ultimate/Enterprise SP1 (64-bit)
  • Windows 10 Professional/Enterprise Version 1607
  • Windows 10 Enterprise 2016 LTSB
  • Windows Server 2016 (64-bit)

The following security programs have been tested with STEP 7 V14 SP1:

  • Virus scanner:
  • Symantec Endpoint Protection 12.1
  • Trend Micro Office Scan Corporate Edition 11.0
  • McAfee VirusScan Enterprise 8.8
  • Kaspersky Anti-Virus 2016
  • Windows Defender (as of Windows 8.1)
  • Qihoo “360 Total Security Essential” 9.7
  • Encryption software:
  • Microsoft Bitlocker
  • Host-based Intrusion Detection System:
  • McAfee Application Control 6.2.0

Ordering data

The products with article numbers (order numbers) are listed in the attached file.

Registrierung notwendig STEP 7 V14 Order list (42.0 KB)

The new TIA Portal / STEP 7 add-on packages included in the list are described in more detail in the following entry: 109744304 

Software Update Service (SUS) as download

All automation software updates on the day of publication, available complete for all applications and independent of location - worldwide! Make the switch to the Software Update Service (SUS) as download now

Trial software download

You can find trial versions for downloading and testing of the several TIA Portal products in the following entries:

  • STEP 7 V14 SP1 109745153 
  • WinCC V14 SP1 109746074 
  • STEP 7 Safety V14 SP1 109746195 
  • Startdrive V14 SP1 68034568 
  • SIMATIC Energy Suite V14 SP1 109746316 
  • SIMATIC Visualization Architect V14 SP1 109746287 
  • SIMOTION SCOUT TIA V5.1 (planned for July 2017)
  • SIMOCODE ES V14 SP1 109745880 (planned for May 2017)
  • Soft Starter ES V14 SP1 109745881 (planned for May 2017)

Readme file

You can find additional information on STEP 7 V14 SP1 Basic/Professional in the attached Readme file.

 Registrierung notwendig  Readme STEP 7 Basic (287,9 KB)

 Registrierung notwendig  Readme STEP 7 Professional (332,7 KB) 

Informational material

TitleLink:
Online Support - Technical information on the TIA Portal65601780
Programming recommendations for S7-1200 / S7-150067582299
Comparison list for programming languages86630375



Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.