×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109746075, Entry date: 03/31/2017
(22)
Rate

Servicepack 2 for SIMATIC WinCC V13 Engineering ( incl. Trial)

  • Entry
  • Associated product(s)
This service pack is applicable for upgrade of the following TIA Portal products: WinCC Basic / Comfort / Advanced / Professional V13 (SP1). Besides providing a series of improvements, the service pack supports installation on Microsoft Windows 10 (March 2017)

As a registered customer, you can download the trial version for  SIMATIC WinCC Basic/Comfort/Advanced/ Professional V14 SP1 and test it for 21 days.

 

New features and changes compared to earlier versions are described in the delivery release for WinCC V13 SP2 

109746073 


Important installation instructions:

The Service Pack 2 available in the entry can be used to upgrade existing V13 installations as well as for new installations.


The TIA Portal products STEP 7 (including PLCSIM), Safety, WinCC, Startdrive and SIMOCODE ES must be upgraded to the same version (V13 SP2). SIMOTION SCOUT TIA must also be upgraded to version V4.4 HF11 (not released for Windows 10).
If the versions are different, the TIA Portal can no longer be started.
Therefore, please make sure you have the service packs of the products you are using before starting the installation. You can find the service packs in the following entries:


  • WinCC V13 Runtime Advanced Servicepack 2 109746268 
  • STEP 7 V13 Servicepack 2 109745155 
  • Startdrive V13 Servicepack 2 109741912
  • Safety V13 SP2 Servicepack 2 109746196
  • SCOUT TIA V4.4 HF11 (not released for Windows 10) 109480713 


Download
 

The software is subject to export restrictions. A download is only possible for registered users. Please note that, on account of the strong demand, the registration for export-restricted downloads will take some time.

The download is split into multiple files. Please first download all of the parts to the same folder and then execute the file with the extension .exe. Afterwards, the parts are merged and you can execute the setup.


WinCC Basic V13 SP2 Trial:

DVD 1: (WinCC Basic V13 SP2)

 Download unterliegt Exportcontrolle  SIMATIC_WinCC_Basic_V13_SP2.exe (2,8 MB)

 Registrierung notwendig  SIMATIC_WinCC_Basic_V13_SP2.001 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Basic_V13_SP2.002 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Basic_V13_SP2.003 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Basic_V13_SP2.004 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Basic_V13_SP2.005 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Basic_V13_SP2.006 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Basic_V13_SP2.007 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Basic_V13_SP2.008 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Basic_V13_SP2.009 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Basic_V13_SP2.010 (222,2 MB)


DVD 2: (Open Source, Tools)

 Registrierung notwendig  SIMATIC_WinCC_Basic_V13_SP2_2.exe (2,8 MB)

 Registrierung notwendig  SIMATIC_WinCC_Basic_V13_SP2_2.001 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Basic_V13_SP2_2.002 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Basic_V13_SP2_2.003 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Basic_V13_SP2_2.004 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Basic_V13_SP2_2.005 (332,1 MB)


SHA-256 checksum:

 Registrierung notwendig  SIMATIC_WinCC_Basic_V13_SP2.txt (2,8 KB)  Information on SHA-256



WinCC Comfort/Advanced V13 SP2 Trial:

DVD 1: (WinCC Comfort/Advanced V13 SP2)

 Download unterliegt Exportcontrolle  SIMATIC_WinCC_Comfort_Advanced_V13_SP2.exe (2,8 MB)

 Registrierung notwendig  SIMATIC_WinCC_Comfort_Advanced_V13_SP2.001 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Comfort_Advanced_V13_SP2.002 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Comfort_Advanced_V13_SP2.003 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Comfort_Advanced_V13_SP2.004 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Comfort_Advanced_V13_SP2.005 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Comfort_Advanced_V13_SP2.006 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Comfort_Advanced_V13_SP2.007 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Comfort_Advanced_V13_SP2.008 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Comfort_Advanced_V13_SP2.009 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Comfort_Advanced_V13_SP2.010 (345,0 MB)


DVD 2: (Open Source, Tools)

 Registrierung notwendig  SIMATIC_WinCC_Comfort_Advanced_V13_SP2_2.exe (2,8 MB)

 Registrierung notwendig  SIMATIC_WinCC_Comfort_Advanced_V13_SP2_2.001 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Comfort_Advanced_V13_SP2_2.002 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Comfort_Advanced_V13_SP2_2.003 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Comfort_Advanced_V13_SP2_2.004 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Comfort_Advanced_V13_SP2_2.005 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Comfort_Advanced_V13_SP2_2.006 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Comfort_Advanced_V13_SP2_2.007 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Comfort_Advanced_V13_SP2_2.008 (247,8 MB)


SHA-256 checksum:

 Registrierung notwendig  SIMATIC_WinCC_Comfort_Advanced_V13_SP2.txt (3,7 KB)  Information on SHA-256


WinCC Professional V13 SP2 Trial:

DVD 1: (WinCC Professional V13 SP2)

 Download unterliegt Exportcontrolle  SIMATIC_WinCC_Professional_V13_SP2.exe (2,8 MB)

 Registrierung notwendig  SIMATIC_WinCC_Professional_V13_SP2.001 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Professional_V13_SP2.002 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Professional_V13_SP2.003 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Professional_V13_SP2.004 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Professional_V13_SP2.005 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Professional_V13_SP2.006 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Professional_V13_SP2.007 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Professional_V13_SP2.008 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Professional_V13_SP2.009 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Professional_V13_SP2.010 (558,3 MB)


DVD 2: (Open Source, Tools)

 Registrierung notwendig  SIMATIC_WinCC_Professional_V13_SP2_2.exe (2,8 MB)

 Registrierung notwendig  SIMATIC_WinCC_Professional_V13_SP2_2.001 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Professional_V13_SP2_2.002 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Professional_V13_SP2_2.003 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Professional_V13_SP2_2.004 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Professional_V13_SP2_2.005 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Professional_V13_SP2_2.006 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Professional_V13_SP2_2.007 (650,0 MB)

 Registrierung notwendig  SIMATIC_WinCC_Professional_V13_SP2_2.008 (247,8 MB)


SHA-256 checksum:

 Registrierung notwendig  SIMATIC_WinCC_Professional_V13_SP2.txt (3,5 KB)Information on SHA-256


Notes for the WinCC Professional installation:


A new WinCC SQL 2014 instance is installed with the installation of WinCC V13 SP2. If you have already installed a version of WinCC Runtime Professional V13 or WinCC Runtime Professional V13 SP1, before you can install WinCC Professional V13 SP2 you must either

  • install WinCC Runtime Professional V13 SP2 first or
  • remove the "WINCC" instance of the SQL Server 2008 R2. (109745000)



Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.