×
Siemens Industry Online Support
Siemens AG
文档类型 软件下载 文档编号 109746196, 文档发布日期 2017年3月31日
(12)
评估

Service Pack 2 for SIMATIC STEP 7 Safety V13 (including TRIAL)

  • 文档
  • 涉及产品
The service pack is valid for upgrading the following products: STEP 7 Safety Basic / Advanced V13 SP1. In addition to a number of improvements, the service pack supports the installation of Microsoft Windows 10.

As a registered customer, you can download Service Pack 2 for SIMATIC STEP 7 Safety Basic / Advanced V13.

Service Pack 2 is used for

  • Upgrading STEP 7 Safety Basic / Advanced V13 (SP1)
  • New installation
  • Can be used for test purposes as a trial version valid for 21 days

In addition to a number of improvements, the service pack supports the installation of Microsoft Windows 10.


System requirements and compatibility with other SIMATIC products

  • STEP7 Safety Advanced V13 SP2 requires STEP 7 Professional V13 SP2 (109745155)  renewed Download available from 16/06/2020
  • STEP 7 Safety Basic V13 SP2 requires at least STEP 7 Basic V13 SP2 (109745155renewed Download available from 16/06/2020


Supported operating systems and hardware requirements can be examined with STEP 7 Professional V13 SP2. The compatibility with other SIMATIC products is the same for STEP 7 Basic / Professional V13 SP2.


Important installation instructions:

All TIA Portal products must be upgraded to the same version (V13 SP2 / SCOUT TIA V4.4 HF11). If the versions are different, you can no longer start the TIA Portal.

Please make sure that the service packs of these products are available before you start the installation. The service packs can be found under the following entries:

  • STEP 7 V13 Service Pack 2 (109745155) renewed Download available from 16/06/2020
  • WinCC V13 Service Pack 2 (109746075)
  • Startdrive V13 Service Pack 2 (109741912)
  • SIMOCODE ES V13 Service Pack 2 (planed for May 2017)
  • SCOUT TIA V4.4 HF11 (not released for Windows 10) (109480713)


Notes about downloading

The software is subjected to export restrictions. Download is only possible for registered users. Please note that, on account of the strong demand, the registration for export-restricted downloads will take some time.


Readme:

You can find additional information on STEP 7 Safety Basic / Advanced V13 SP2 in the included Readme file. You can view this file in the portable document format (.pdf):

 Registrierung notwendig  ReadmeFAILenUS_V13_SP2.pdf (284,4 KB)


SIMATIC STEP 7 Safety Basic / Advanced V13 SP2 (03/2017):

Download unterliegt Exportcontrolle STEP_7_Safety_V13_SP2.exe (230.6 MB)

SHA-256 checksum: Registrierung notwendig STEP_7_Safety_V13_SP2.txt (1 KB)

You can find additional information about SHA-256 here.





安全性信息
为了保护技术基础设施、系统、机器和网络免受网络威胁,有必要实施并持续维护一个全面、最先进的IT安全方案。西门子的产品和解决方案构成了这一方案的一个要素。有关网络安全的更多信息,请访问
https://www.siemens.com/cybersecurity#Ouraspiration.
评估文档
无评估
请求和反馈
您想要做什么?
注意:反馈总是与当前的条目/产品相关。您的消息将被转发给我们在线支持团队的技术编辑们。如果我们需要就您的反馈提供答复,您将在几天内收到答复。如果没有其它问题,您将不会收到答复。