×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109746276, Entry date: 03/31/2017
(12)
Rate

Servicepack 1 für SIMATIC WinCC V14 Runtimes (TIA Portal)

  • Entry
  • Associated product(s)
Servicepack 1 available for WinCC V14

The Service Pack is applicable to the following products: 

  • WinCC Runtime Advanced V14
  • WinCC Runtime Professional V14  oder V14 ASIA
  • WinCC Runtime Client V14 oder V14 ASIA

 

New features and changes compared to earlier versions are described in the delivery release for WinCC V14 SP1 109745460


Important installation instructions:


The TIA Portal products STEP 7 (including PLCSIM), Safety, WinCC, SIMATIC Energy Suite, SiVArc, Startdrive, SIMOCODE ES and Softstarter ES must be upgraded to the same version (V14 SP1). SIMOTION SCOUT TIA must also be upgraded to version V5.1.


If the versions are different, the TIA Portal can no longer be started.
Therefore, please make sure you have the service packs of the products you are using before starting the installation. You can find the service packs in the following entries: 


  • WinCC V14 Engineering Servicepack 1 109746074
  • Step 7 V14 Servicepack 1 109745153
  • Startdrive V14 Servicepack 1 109746259 
  • Safety V14 Servicepack 1 109746195
  • SiVArc V14 Servicepack 1 109746287
  • Energy Suite V14 Servicepack 1 109746316
  • SIMOCODE ES V14 Servicepack 1 109745880 (planed for 05/2017)
  • Softstarter ES V14 Servicepack 1 109745881  (planed for 05/2017)
  • SCOUT TIA V5.1 (planed for 07/2017)


Download

The software is subject to export restrictions. A download is only possible for registered users. Please note that, on account of the strong demand, the registration for export-restricted downloads will take some time. 

The download is split into multiple files. Please first download all of the parts to the same folder and then execute the file with the extension .exe. Afterwards, the parts are merged and you can execute the setup.

The free download contains the service pack 1 for upgrading existing installations of WinCC Runtime V14 and can only be installed if WinCC Runtime V14 is already installed.

The DVD has to be ordered to support the new operating systems (Windows 10 and Windows Server 2016).

Order number:

 6AV2104-0XX04-0DU8SIMATIC WinCC Runtime Advanced  V14 SP1 Update V14 -> V14 SP1 
 6AV2105-0XX04-0DU8SIMATIC WinCC Runtime Professional  V14 SP1 Update V14 -> V14 SP1 


Servicepack 1 for WinCC Runtime Advanced V14:


 Download unterliegt Exportcontrolle  SIMATIC_WinCC_Runtime_Advanced_SP1_for_V14.exe (1,1 GB)


SHA-256 checksum:


 Registrierung notwendig  SIMATIC_WinCC_Runtime_Advanced_SP1_for_V14.txt (1 KB) Information on SHA-256


Servicepack 1 for WinCC Runtime Professional V14:

 Download unterliegt Exportcontrolle  SIMATIC_WinCC_Runtime_Professional_SP1_for_V14.exe (2,8 MB)

 Registrierung notwendig  SIMATIC_WinCC_Runtime_Professional_SP1_for_V14.001 (2,0 GB)

 Registrierung notwendig  SIMATIC_WinCC_Runtime_Professional_SP1_for_V14.002 (2,0 GB)

 Registrierung notwendig  SIMATIC_WinCC_Runtime_Professional_SP1_for_V14.003 (564,6 MB)


SHA-256 checksum:

 Registrierung notwendig  SIMATIC_WinCC_Runtime_Professional_SP1_for_V14.txt (1 KB) Information on SHA-256





Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.