×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109746396, Entry date: 10/19/2017
(2)
Rate

Which Mettler Toledo weigh modules can be connected with SIWAREX FTA, SIWAREX FTC und SIWAREX WP231 and how is commissioning carried out?

  • Entry
  • Associated product(s)

Question:

Which Mettler Toledo weigh modules can be connected with SIWAREX FTA, SIWAREX FTC und SIWAREX WP231 and how is commissioning carried out?

Answer:

The weighing modules SIWAREX FTA, SIWAREX FTC and SIWAREX WP231 can be connected to several weigh modules from Mettler-Toledo. The possible combinations of the products as well as an installation instruction can be found on the Mettler Toledo web page.

Documentation for SIWAREX FTA and SIWAREX FTC:
https://www.mt.com/dam/ind/MTA/Platforms/DataSheet/New_K-Line/PBK/EN221_PBK9-PFK9-APW_and_SIWAREX-FTA-FTC.pdf

Documentation of SIWAREX WP231: http://www.mt.com/dam/ind/MTA/Platforms/DataSheet/New_K-Line/PBK/EN181_PBK9-PFK9-APW_and_SIWAREX-WP231.pdf

Descriptions for SIWAREX WP231 can also be found in the user manual in the respective chapters under https://support.industry.siemens.com/cs/ww/en/view/109738522


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.