×
Siemens Industry Online Support
Siemens AG
Entry type: Product note, Entry ID: 109746402, Entry date: 03/31/2017
(0)
Rate

No 10 Mbps data transfer with SCALANCE XC-100

  • Entry
  • Associated product(s)
The following situation arises when end devices with a 10-Mbps interface are connected to the Industrial Ethernet Switches of the SCALANCE XC-100 product family: The switch establishes a link to the end devices, indicated by the green LED at the switch, but no data transfer takes place.

The following article numbers are affected:


Product name

Article no.

Product version

SCALANCE XC106-2

6GK5106-2BB00-2AC2

01

SCALANCE XC106-2

6GK5106-2BD00-2AC2

01

SCALANCE XC108

6GK5108-0BA00-2AC2

01

SCALANCE XC116

6GK5116-0BA00-2AC2

01

SCALANCE XC124

6GK5124-0BA00-2AC2

01



Information concerning replacement

The solution is available in the form of a new product version. If replacement is necessary, please contact the sales contact oerson responsible for you.


Transmission of 100 mbps works without issues.