×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109746436, Entry date: 11/20/2017
(2)
Rate

Firmware Update for ET 200MP F-DQ 8x24VDC 2A PPM

  • Entry
  • Associated product(s)
Firmware Update for ET 200MP F-DQ 8x24VDC 2A PPM


Description:

When firmware is updated, it must always be updated to the latest version available for the relevant article number.

A detailed description of the firmware update procedure is provided in the entry109742293.

Overview of article numbers and current firmware version of ET 200MP F-DQ 8x24VDC 2A PPM:

Article number

Software
version

Upgrade by means of...

6ES7526-2BF00-0AB0
V1.0.2

Recommended for upgrade:
See description Update V1.0.2

Note: The firmware is subject to export restrictions, download only for registered users


For STEP 7 TIA Portal
 Download unterliegt Exportcontrolle  TIA_6ES7526-2BF00-0AB0_V102.ZIP (206,3 KB)
SHA-256 checksum (Information on SHA-256)
 Registrierung notwendig  TIA_6ES7526-2BF00-0AB0_V102.txt (1 KB)


Update V1.0.2

The following behavior was modified:

The communication error diagnostic message which can result in passivation was output highly sporadically for this module. This behavior has been corrected in firmware version V1.0.2.


Update V1.0.1

The following behavior was modified:

The restrictions on parameter settings have been eliminated.
See PI for V1.0.0.109482428




Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.