×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109746466, Entry date: 04/04/2017
(9)
Rate

SINAMICS Startdrive V14

  • Entry
  • Associated product(s)
You can find the Startdrive version V14 here.

SINAMICS Startdrive V14

OSS note on SINAMICS Startdrive V14

Third-party software - license conditions and copyright notes
You can find the copyright notes on the third-party software, especially Open Source Software, as well as applicable license conditions for this type of third-party software in the following file:

 Registrierung notwendig  ReadMe_OSS_all_languages.htm (1,5 MB)

Special note for resellers
The information and the license conditions in the ReadMe_OSS.htm file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

OSS Source Code
The source code files are part of the download package.

Note
Only one download package is available for Startdrive V14. The subdivision into two separate download packages for “Option package for STEP 7“ and “Startdrive Standalone“ is no longer necessary. Startdrive V14 suppprts both installation variants.

Here you can find the Startdrive commissioning tool for the SINAMICS G120 drive Family.

SINAMICS Startdrive V14
SINAMICS Startdrive V14

Associated sales information you can find here 109736502 

 Registrierung notwendig  Startdrive_V14.zip (2,3 GB)

SHA-256-checksum: 

FDE0AD9E4383B82689CD97F0C84F06134968104179A75C48D66831DF92AE0FB0

SINAMICS Startdrive V14 Update 2

Associated sales information you can find here 109743597 

 Registrierung notwendig  Startdrive_V14_Update_2.zip (1,7 GB)

SHA-256-Prüfsumme: 

9B5A1613C93A4F4A772A7D2C21DB402EE9123E21F6C12CD38FC2097AC8B747C7


Use of SINAMICS Startdrive is free of charge and does not require a license key to be entered.

Startdrive supports the languages German, English, French, Spanish, Italian and Chinese (simplified).

How to install Startdrive V14:

  1. Download the attached ZIP file
  2. Unpack the ZIP file into a target directory on your hard disk. Pleae make sure that no spaces are contained in the entire path name of this target directory.
  3. Launch Startdrive using Start.exe.


Notes regarding the download

Because of the security settings, the download may be classified as a security risk as shown in the screenshot.
In order to avoid problems after the installation, ZIP files must be classified as safe after the download by
right-clicking > Properties > "Allow" button.


Additional search terms
FB284, FB285, FB286, blocks, SINA_POS, SINA_SPEED, SINA_PARA
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.