×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109746504, Entry date: 04/06/2017
(3)
Rate

Delivery release for SINAMICS Startdrive V14 SP1 Update 1

  • Entry
  • Associated product(s)
Update 1 for Startdrive V14 SP1 has been released for delivery.

Update 1 for Startdrive V14 SP1 is available under 68034568 and includes the following improvements:

  • Mask of analog inputs

    • Correction of the restriction TFS-RQ 2202251:
      TIA-portal crashes in online mode at changing the value of "analog input type" (p756[0]) on the mask "inputs/outputs"\"Analog inputs" of the functional view.

  • Masks of basic positioner

    • Correction of the restriction TFS-RQ 2202757:
      TIA-portal freezes while navigating through the masks of basic positioner in functional view. 

Installation instructions

  • The update can only be installed if Startdrive V14 SP1 has already been installed.
  • After each installation of Startdrive V14 SP1, the update needs to be installed. 
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.