×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109746557, Entry date: 06/19/2017
(1)
Rate

SIMOTICS S-1FG1 geared motors: Sales and delivery release for the options Q94, Q95 and Q96

  • Entry
  • Associated product(s)
With the options Q94, Q95 and Q96 you can define the position of the manual release lever, including air gap control.

Update 2018-07-10: possible positionen manual brake release (see table)

The options Q94, Q95 and Q96 define the position of the manual release lever and the air gap control (K82) with spring-applied brakes (N30 to N34) which are always located on the same side.

Selection options

  • Standard = Manual brake release lever top
  • Q94 = Manual brake release lever, on the right
  • Q95 = Manual brake release lever bottom
  • Q96 = Manual brake release lever, on the left




NOTICE

With the newly introduced options, the article number is changed compared to the previous one.

Old

The manual release lever was located at the same position as the connecting plug, that means, with the selected position of the plug at the bottom (option Q92), the manual release lever was also located at the bottom.

New

The position of the manual release lever must be selected separately with the options Q94, Q95, Q96 or in the standard above (without stating an option), that means, in the above-mentioned example, you must additionally select the option Q95 to ensure that the manual release lever is also located at the bottom.

Restriction

The position of the manual release lever is limited due to construktion reasons (see table).

Possible lever position motor shaft height 80 mm ("E" - 10th place of the artikel number):   X
Possible lever position motor shaft height 100 mm ("F" - 10th place of the artikel number):  X and (X)

Connector topQ91Q92Q93
Lever
top X(X)X-
Q94 -X(X)X
Q95 X-X(X)
Q96 (X)X-X


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.