×
Siemens Industry Online Support
Siemens AG
Entry type: Product note, Entry ID: 109747482, Entry date: 05/12/2017
(2)
Rate

Sales/delivery release for SIMATIC NET DVD V14 + SP1

  • Entry
  • Associated product(s)
Effective immediately, the following service pack for the SIMATIC NET PC software products (e.g. SOFTNET-IE S7, SOFTNET-PN IO, S7 REDCONNECT) has been released for sale and delivery: SP1 for the SIMATIC NET DVD V14

The service pack contains qualitative improvements as compared to the basic V14 versions.

In addition, the operating system Windows 10 (Pro/Enterprise) 64-bit as of version 1511, Build 10586.36 is supported.

Please make sure to observe the following:

The MLFBs for the products remain unchanged. Licenses (with the associated license keys) for the basic versions are also valid for the service pack.

Delivery is in the form of product packages.

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.