×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109747494, Entry date: 07/10/2018
(0)
Rate

SIRIUS ACT PROFINET configuration with STEP 7 Classic or TIA Portal

  • Entry
  • Associated product(s)
This article contains information on configuring with STEP 7 Classic or TIA Portal.

QUESTION:

How can SIRIUS ACT with PROFINET be parameterized in STEP 7 Classic or TIA Portal?

 

 

ANSWER:

SIRIUS ACT with PROFINET can be parameterized in STEP 7 Classic or TIA Portal as follows.

STEP 7 Classic
The 3SU1 Standard interface module (IM)  can be parameterized in STEP 7 Classic (e.g. V5.5) only with GSDML.

You can find the GSDML file for the Standard interface modules online at the following link.

The
  3SU1 Failsafe interface modules (IM-F) cannot be incorporated into STEP 7 Classic as the F address cannot be assigned. The F address can only be assigned via TIA Portal V13/V14.
In the case of SIRIUS ACT with PROFINET, the F address is assigned via the software (F address assignment), not via a DIP switch as for other products. F address assignment is only possible in the TIA Portal.
For this reason, there is only one GSDML for the Standard interface module 3SU1400-1LK10-.AA1, but not for the Safety interface module 3SU1400-1LL10-.BA1.


TIA V13 / V14
The 3SU1 Standard interface module (IM)  and 3SU1 Failsafe interface module (IM-F) can be parameterized in TIA (e.g. V13/V14) with the relevant HSP.

The HSP for the interface modules (IM + IM-F) can be found online at the following link.