×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109747521, Entry date: 05/29/2017
(5)
Rate

SINAMICS Startdrive V14 SP1 Update 3

  • Entry
  • Associated product(s)
Update 3 for Startdrive V14 SP1 has been released for delivery.

Update 3 for Startdrive V14 SP1 is available under68034568 and includes the following improvements:

  • Modified behavior of the drive control panel:
When activating the drive control panel (backwards/forwards), the direction of rotation can be selected before starting the motor. This change supports scenarios with a vertical load application during which the load slightly moves downwards when starting the motor.

Previous updates

  • The update is cumulative and contains all previous Startdrive V14 SP1 updates.

Installation instructions

  • The update can only be installed if Startdrive V14 SP1 has already been installed.

  • After each installation of Startdrive V14 SP1, the update needs to be installed.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.