×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109747569, Entry date: 05/31/2017
(0)
Rate

New options and country-specific approvals for the SIMATIC Industrial Tablet PC (ITP1000)

  • Entry
  • Associated product(s)
With immediate effect, further options can be ordered for SIMATIC ITP1000. These include a Celeron CPU, 16GB DDR4 RAM, as well as further country-specific power cables. The radio approvals and country certificates for the USA / Canada are also available with immediate effect.

New ordering options

With immediate effect, further ordering options are available for the SIMATIC Industrial Tablet PC. A cost-efficient Celeron CPU (Intel® Celeron® Processor G3902E, 1.6 GHz, 2M Cache) is now also available for less demanding tasks. Further, you can also order SIMATIC ITP1000 with 16 GB DDR4 RAM for particularly memory-intensive applications in the future. The selection of power cables is extended as follows:

  • Specific cable for Switzerland
  • Specific cable for the UK
  • Specific cable for the USA
  • Specific cable for Italy

Further radio approvals and certificates

With immediate effect, SIMATIC ITP1000 has also been released for use on the US / Canadian market. Thus, SIMATIC ITP1000 provides the following certificates and radio approvals:

  • CE
  • UL
  • CSA
  • RoHS II
  • EuP / ErP
  • FCC
  • IC


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.